2023-02-25 6:49 AM
I have configured the readout of 4 PDM microphones through the SAI interface. I am using 1 slot of 32 bits per frame.
I have enabled DMA.
Unfortunately, when reading PDM data, the first 6 and last 2 values of the array are filled with zeros. This happens regardless of the size of the PDM_buffer.
Do I have something misconfigured? What could be the cause?
Edit: If the PDM_buffer array is of type uint16_t, there are 2x more zeros (12+4 ), and in the case of uint8_t 4x more zeros (24+8).
2023-10-08 11:50 PM
OK, I tried different things, I read many articles about similar problems, but I can't deal with it. Is there any relatively simple way to deal with DCache support? Can you show me step by step what I should change and in which files, or what I should add in my program to make DCache work properly?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.