2011-12-13 2:24 PM
Has anyone been able to use the DAC output (PA4) to generate sound on the headphone port? It seemed like a trivial thing to do, set up the CS43L22 in analog pass-thru mode... but that was 3 days ago. I generate a 3.5kHz sine wave on PA4 and can scope it all the way to the Cirrus CS43L22 but nothing I have programmed to it over the I2C has worked. I even downloaded the scripts to Cirrus' eval board and mimic'd them in my code's I2C comands and that did not work.
I know the CS43L22 is alive because I was able to compile and run an abbreviated vesion of the Audio_playback_and_record demo. I tried modifying waveplayer.c to choose the AUDIO_INTERFACE_DAC... no luck. Any insights would be appreciated. By the way, the way the Discovery is configured (2.5V on the CS43L22 and 3.3V on the STM32F4 DAC) appears to apply a voltage above the max rating on the analog in (AIN1A & AIN1B) pin of the CS43L22... maybe I accidently smoked the analog input by using the DAC at full range... THANKS... #stm32f4discovery-dac-audio2012-02-11 6:07 PM
Found the code in stm32f4_discovery_audio_codec.c
GBWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.