STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4-Firmware Library

Posted on November 23, 2011 at 18:55Hi,Does anyone find the user manual that describes firmware library?Because for STM32F101xx and STM32F103xx this manual exist, and its very helpfull, without this we complicated to know the all functions!Best Rega...

10408892 by Associate
  • 1953 Views
  • 4 replies
  • 0 kudos

STM32_USB-FS-Device_Lib_V3.3.0 on the STM32F4

Posted on February 13, 2012 at 12:54This is a preemptive question as I have not had anytime to look into this yet but it crossed my mind while building my project.I am currently working on a project destined to go onto my own board with a STM32F417 ...

eamonn by Associate II
  • 814 Views
  • 0 replies
  • 0 kudos

STM32 with multiple CAN ports

Posted on February 09, 2012 at 10:59Is there any plans to release an STM32F2 or F4 with 3 or 4 CAN ports?   Any ideas on adding external CAN ports if not?    #can-stm32f2-stm32f4

USART and DMA (for RS485)

Posted on January 16, 2012 at 16:56 Hello all, I am using DMA to manage the TX line of one USART (RX stays on standard interrupt). I have no problem with a RS232 tranceiver. But when I use a RS485 tranceiver I got a problemwith the CBUS ...

Serial data from GPS to Bluetooth via STM32F103

Posted on February 09, 2012 at 11:18Hi all,I am looking for suggestions on how to design the data forwarding between a GPS receiver and a BT transceiver. It is a https://picasaweb.google.com/111166516525827756469/Rappen10LogBt&sharp57050240279869343...

michele77 by Associate II
  • 2183 Views
  • 4 replies
  • 0 kudos

Fatal error-NO MCU found?

Posted on February 11, 2012 at 21:44Last night I was working with my STM32L and everything was working properly. I had loaded some code to flash the leds. I had the board set up on a bread board and was using the the external 3v power supply pins to...

rj by Associate II
  • 2624 Views
  • 5 replies
  • 0 kudos

DAC to Audio Out

Posted on December 13, 2011 at 23:24Has anyone been able to use the DAC output (PA4) to generate sound on the headphone port? It seemed like a trivial thing to do, set up the CS43L22 in analog pass-thru mode... but that was 3 days ago. I generate a ...

dreschel by Associate II
  • 1183 Views
  • 1 replies
  • 0 kudos

Flash programming error in Keil MDK

Posted on February 11, 2012 at 16:27Hi! I just started using the STM32F4 discovery board with Keil development environment, and I have a small problem, that I can not program the flash memory of the microcontroller using the Load button. In Keil Bui...

miklos by Associate II
  • 2883 Views
  • 2 replies
  • 0 kudos

u32 should be alligned ?

Posted on February 11, 2012 at 01:17hello One question: when i am using: char table[10]; (...) *(unsigned int*)&table[1]=0x12345678; should the pointer be dword alligned in RAMy ? Can I make safely such access? Or it is forbidden in ARM architecture...

wadi by Associate II
  • 856 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.