2009-07-26 5:30 AM
DAC Programmation
2011-05-17 4:18 AM
Hello,
For my firt application, I want to use DAC. My aim is to send a constant value on the pin DAC_OUT1 (pin 20) by using channel 1 of the DAC. I made this code : #include ''stm32f10x_lib.h'' #include ''stm32f10x_conf.h'' #include ''stm32f10x_map.h'' #include ''stm32f10x_dac.h'' int main(void){ DAC_DeInit(); DAC_InitTypeDef DAC_InitStructure; DAC_InitStructure.DAC_Trigger = DAC_Trigger_None; DAC_InitStructure.DAC_WaveGeneration = DAC_WaveGeneration_None; DAC_InitStructure.DAC_LFSRUnmask_TriangleAmplitude = DAC_LFSRUnmask_Bit0; DAC_InitStructure.DAC_OutputBuffer = DAC_OutputBuffer_Enable; DAC_Init(DAC_Channel_1, &DAC_InitStructure); DAC_Init(DAC_Channel_2, &DAC_InitStructure); DAC_Cmd(DAC_Channel_1, ENABLE); DAC_Cmd(DAC_Channel_2, ENABLE); DAC_DMACmd(DAC_Channel_1, DISABLE); DAC_DMACmd(DAC_Channel_2, DISABLE); DAC_SoftwareTriggerCmd(DAC_Channel_1, DISABLE); DAC_SoftwareTriggerCmd(DAC_Channel_2, DISABLE); DAC_DualSoftwareTriggerCmd(DISABLE); DAC_SetChannel1Data(DAC_Align_12b_L, 0x500); DAC_SetChannel2Data(DAC_Align_12b_L, 0x400); USART_SendData(USART1, DAC_GetDataOutputValue(DAC_Channel_1)); USART_SendData(USART2, DAC_GetDataOutputValue(DAC_Channel_2)); } Firstly, I have a questions, My code is good ? I use too much function or not ? Are the data will be send on the DAC_OUTPUT1 ? (Using usart is just for simulation on debug mode) Secondly, I have a problem, The USART DATA REGISTERs 1 and 2 indicate 0x1ff although we must have 0x500 for USART1 and 0x400 for USART2. (DAC data and USART data use the same type : u12) So if someone have an idea. I will be happy. Thanks, JC.2011-05-17 4:18 AM
Hi,
You can start using the DAC examples provided in the Firmware Library : http://www.st.com/stonline/products/support/micro/files/stm32f10x_stdperiph_lib.zip and then tailor to your application. Cheers, STOne-32.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.