2018-10-19 2:03 AM
Hi,
what is the correct way to initialize the MAC address read from an external memory by using LwIP?
/* Initialize all configured peripherals */
..
=> need MAC address here do correct initalization...
MX_LWIP_Init();
...
=> MAC address can be read here from SPI flash or similar...
MX_SPI2_Init();
MX_SPI1_Init();
...
my suggest (but not possible within user code sections):
/* Initialize all configured peripherals */
...
=> MAC address can be read here from SPI flash or similar...
MX_SPI2_Init();
MX_SPI1_Init();..
...
/* USER CODE BEGIN READ MACADDRESS */
=> USER CODE SECTION could be useful here to read MAC address from external memory
/* USER CODE END READ MACADDRESS */
...
MX_LWIP_Init();
...
thanks
2018-10-19 2:52 AM
In my experience, manufacturers most often avoid the costs of external chips, and rather patch the MAC address (or other specific data) into the HEX file.
2018-10-19 3:18 AM
Thanks,
but however, I have to read out MAC Address from an external memory. If an firmware update has to be done, I can't patch all the HEX files individually.
Perhaps others have the same problem?
best reagrds
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.