2018-01-31 2:17 AM
Hello everyone,
after update of STM32CubeMX it started to generate simply uncompilable code for TrueSTUDIO.
When I select FATFS od FREERTOS and TrueSTUDIO as a IDE, after compilation,
functions like HAL_Init(), osThreadCreate(), osKernelStart(), HAL_RCC_OscConfig(), HAL_SD_ReadBlocks_DMA()
and similar are marked with errors 'Undefined reference'.
However when I choose only SDIO, all HAL functions are compiled without problems.
I've got Atollic TrueSTUDIO® for STM32 v9.0.0, hovewer I don't think that problem is in IDE.
When I generate code in CubeMX code for MDK-ARM v5, everything compiles without problem.
From attached projects, only SAMPLE_SDIO.ioc works.
Does someone have similar problem?
Solved! Go to Solution.
2018-02-26 1:00 AM
2018-03-20 9:31 AM
Hello all,
This issue is now fixed in the current CubeMX release.
Please, upgrade with CubeMX4.25 if not already done.
BR. Jeanne
2019-03-08 4:08 AM
Here is my workaround:
create a project with cubeMx and the uC of your choice. Then only change in "project Manager" toolchain, directory and project location. Dont assign any pins or make a configuration! Just genereate the project , open it in atollic and it should be compileable.
When i assigned Pins and did some configuration, the generated project was not compilable in Atolloc
Using Cube 5.01 and Atollic 9.1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.