2016-06-03 1:35 PM
Hi everybody,
I have some issue with using the DMA Transfer method on a Discovery F3 (F303) board. Don't know if it's a bug, or if I missed something... The HAL is generated with Cube (under Eclipse, Cube-Version is STM32Cube_FW_F3_V1.4.0). Following issue: I start a DMA-Receive (Mainclass.cpp, line 81), which is continuously restarted within the HAL_UART_RxCpltCallback (yes, I should try circular mode). When a button-press occours I want to send some string-message. This works fine - but only one time. Snippet (Mainclass.cpp, line 110): if (last_key == '#') { strncpy((char*) uart_tx_buffer, (const char*) ''oans, zwoa, gsuffa..'', uart_tx_buffer_len); HAL_UART_Transmit_DMA(uart, uart_tx_buffer, uart_tx_buffer_len); } Problem is, that after transmission the UART-State stays ''BUSY_RX_TX''. This prevents further transmissions. Maybe I should set the state by my own software, but no IRQ is called where I could do this. A look into UART_DMATransmitCplt (file stm32f3xx_hal_uart.c) shows the enabling of some IRQ. But no IRQ is ever called. Line 1848: /* Enable the UART Transmit Complete Interrupt */ __HAL_UART_ENABLE_IT(huart, UART_IT_TC); Workaround may be to use circular mode and stop transmission in the HAL_UART_TxCpltCallback? So - which IRQ is enabled by line 1848 (or should be enabled)? Did I miss something? Source files will be attached later. Thank you EDIT: I didn't manage to attach files. Blocked by administrator...2016-06-03 2:34 PM
(Cool. My first post was swallowed, my second one echoed several times.)
I played around with some settings in Cube - got it. The global Interrupt on USART1 must be enabled. Works now!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.