2020-03-02 11:17 AM
Hi everyone,
I have recently starting becoming familiar with the M-Cortex structure and instruction set ( I was raised on Atmel MCUs in school and this is my first time working with M-Cortex and .thumb instructions) I am trying to learn as much as I can, but there is an impressive amount to learn. So, I have decided to just take it in small chunks as problems become relevant. I want to put a simple program (flash LED) out in an external QSPI flash part on a custom board. I was able to modify the SEGGER project for my part to get the QSPI to execute the erase and program functions properly and I can successfully erase through Jlink commander now. I think at this point I could get my program out into the external flash but my question is how do I get to the external flash on reset? I found and external memory example but it runs out of RAM to init QSPI and write to it from a UART. This makes sense to me from the perspective of trying to get something into external when either using a debugger to program or some other interface like USB, but what about when that device is removed and reset occurs? Wouldn't there need to be a bootloader-esque function pointer in internal flash to hand execution off to the program in external upon exiting the reset handler?
I am using IAR EWARM and I also found *.icf for linker scripts. I was thinking I could have a script that would know to stitch together my application and my bootloader in one executable. So, I would have my app put at the start for external flash and my bootloader in internal flash. Does this make sense or am I off the yellow brick road? I just have to figure out how to indicate that with IAR because it seems to want to produce an executable with a linker involved in project settings. I was thinking I would just have a *.bin (or something) that could be called into use with another linker script that would be for my application.
Sorry for the long post. I am new to this so I haven't created a solid picture or had much reinforcement on some of the stuff I am learning. Thanks in advance!
2020-03-02 8:33 PM
Sounds like you have a reasonable grasp of the issues.
The code to stand up the QSPI interface and pins needs to be in the Internal Flash, it can then access the external memory and transfer control to it.
You could split resources between the internal and external memories via the linker script or .ICF file for IAR. You would just have to be careful about not creating any dependencies on the external memory before it is initialized.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.