2020-08-07 6:56 AM
Hey Guys, iam trying to convert Arduino Code to my C Project in CubeIDE..
I have some troubles(=warnings and iam unsure) with the SPI Trasmit functions.
Could you tell me if my code does the same as the Arduino Code?
ARDUINO :
*******************
void SX126XLT::readRegisters(uint16_t address, uint8_t *buffer, uint16_t size)
{
#ifdef SX126XDEBUG
//Serial.println(F("readRegisters()"));
#endif
uint16_t index;
uint8_t addr_l, addr_h;
addr_h = address >> 8;
addr_l = address & 0x00FF;
checkBusy();
#ifdef USE_SPI_TRANSACTION //to use SPI_TRANSACTION enable define at beginning of CPP file
SPI.beginTransaction(SPISettings(LTspeedMaximum, LTdataOrder, LTdataMode));
#endif
digitalWrite(_NSS, LOW);
SPI.transfer(RADIO_READ_REGISTER);
SPI.transfer(addr_h); //MSB
SPI.transfer(addr_l); //LSB
SPI.transfer(0xFF);
for (index = 0; index < size; index++)
{
*(buffer + index) = SPI.transfer(0xFF);
}
digitalWrite(_NSS, HIGH);
#ifdef USE_SPI_TRANSACTION
SPI.endTransaction();
#endif
}
void SX126XLT::writeRegisters(uint16_t address, uint8_t *buffer, uint16_t size)
{
#ifdef SX126XDEBUG
//Serial.println(F("writeRegisters()"));
#endif
uint8_t addr_l, addr_h;
uint8_t i;
addr_l = address & 0xff;
addr_h = address >> 8;
checkBusy();
#ifdef USE_SPI_TRANSACTION //to use SPI_TRANSACTION enable define at beginning of CPP file
SPI.beginTransaction(SPISettings(LTspeedMaximum, LTdataOrder, LTdataMode));
#endif
digitalWrite(_NSS, LOW);
SPI.transfer(RADIO_WRITE_REGISTER);
SPI.transfer(addr_h); //MSB
SPI.transfer(addr_l); //LSB
for (i = 0; i < size; i++)
{
SPI.transfer(buffer[i]);
}
digitalWrite(_NSS, HIGH);
#ifdef USE_SPI_TRANSACTION
SPI.endTransaction();
#endif
}
***************
c in CubeIDE :
***************
void readRegisters(uint16_t address, uint8_t *buffer, uint16_t size)
{
#ifdef SX126XDEBUG
uint8_t s[] ="readRegisters() \r\n";
tx_com(s, strlen((char const*)s));
#endif
uint16_t index;
uint8_t addr_l, addr_h;
addr_h = address >> 8;
addr_l = address & 0x00FF;
checkBusy();
HAL_GPIO_WritePin(SX1261_NSS_GPIO_Port, SX1261_NSS_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, RADIO_READ_REGISTER, sizeof(RADIO_READ_REGISTER), HAL_MAX_DELAY);
HAL_SPI_Transmit(&hspi1, addr_h, sizeof(addr_h), HAL_MAX_DELAY);
HAL_SPI_Transmit(&hspi1, addr_l, sizeof(addr_l), HAL_MAX_DELAY);
HAL_SPI_Transmit(&hspi1, 0xFF, sizeof(0xFF), HAL_MAX_DELAY);
HAL_SPI_TransmitReceive(&hspi1, 0xFF, buffer, size, HAL_MAX_DELAY);
HAL_GPIO_WritePin(SX1261_NSS_GPIO_Port, SX1261_NSS_Pin, GPIO_PIN_SET);
}
void writeRegisters(uint16_t address, uint8_t *buffer, uint16_t size){
#ifdef SX126XDEBUG
uint8_t s[] ="writeRegisters() \r\n";
tx_com(s, strlen((char const*)s));
#endif
uint8_t addr_l, addr_h;
addr_l = address & 0xff;
addr_h = address >> 8;
checkBusy();
HAL_SPI_Transmit(&hspi1, RADIO_WRITE_REGISTER, sizeof(RADIO_WRITE_REGISTER), HAL_MAX_DELAY);
HAL_SPI_Transmit(&hspi1, addr_h, sizeof(addr_h), HAL_MAX_DELAY); //MSB
HAL_SPI_Transmit(&hspi1, addr_l, sizeof(addr_l), HAL_MAX_DELAY); //LSB
HAL_SPI_Transmit(&hspi1, buffer, size, HAL_MAX_DELAY);
HAL_GPIO_WritePin(SX1261_NSS_GPIO_Port, SX1261_NSS_Pin, GPIO_PIN_SET);
}I dont know if iam using the right functions and if i have the right arguments .
Esspecially the 2nd Argument in the HAL_SPI_Transmit(); function ..
CubeIDE gives me a warning : makes pointer from integer without a cast [-Wint-conversion]
thank you
2020-08-10 6:22 AM
what if i dont want to change the function body?
ptr could already be a pointer ? or am i thinking wrong?
i did not work a lot with pointers (or call by reference in general) I just looked it up in the textbook and iam confused..
lets look at that example:
uint8_t tx_buffer[] = { 0xFF };
HAL_SPI_Transmit(&hspi1, tx_buffer, sizeof(tx_buffer), HAL_MAX_DELAY);the function body of HAL_SPI_Transmit looks like this :
HAL_StatusTypeDef HAL_SPI_Transmit (SPI_HandleTypeDef * hspi, uint8_t * pData, uint16_t Size, uint32_t Timeout)
looking at this i think SPI_Transmit needs a pointer to the data to transmit. Doesnt that mean i have to call it with & ?
like this: ?
uint8_t tx_buffer[] = { 0xFF };
HAL_SPI_Transmit(&hspi1, &tx_buffer, sizeof(tx_buffer), HAL_MAX_DELAY);The function gets
CubeIDE gives me a incompatible Pointer warning when i try that ..
would be super nice if you could explain that to me...
thanks!
2020-08-10 6:32 AM
2020-08-10 6:36 AM
void startWriteSXBuffer(uint8_t ptr) {
[...]
HAL_SPI_Transmit(&hspi1, &ptr, 1 , HAL_MAX_DELAY);
}what about that ? size is 1 because its only an uint8_t ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.