2020-06-16 6:54 AM
I created a project using the CubeMX software, as the basis for a music playing device.
I then used the SD disk io dma rtos driver from the wav player/recorder as the cube generated code is broken.
Can I put a project on github using the above code?
I've left the copyright agreements in place, but perhaps modified header references in places. Can anyone (perhaps an ST rep) provide guidance here?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.