2013-02-12 1:33 PM
I have a boot loader that resides in the first flash block of an STM32F4 family processor which is 16K begining at 0x08000000. I would like the last four byte of the sector at 0x08003ffc to contain constant data representing a version number.
Any suggestions? I am using Atollic tools which are GCC based. I would prefer a C/C++ solution but could use assembler if necessary. My current knowlege of ARM assembly is fairly limited. John2013-02-12 1:52 PM
Any suggestions?
Specify an address, or memory/section in the linker script, and define the ''attributes'' of the variable to direct it's placement. Google some documentation and examples for GNU linker scripts.2013-02-13 7:40 AM
Thanks. If I make one section just for the version, that should work.
John2013-02-13 1:29 PM
I used the interupt vectors as an example for the linker file (to define a section similar to
.isr_vector
) and the startup.s file (to defined data within the section as is done with the vector table). The defined values showed up in the s-record at the expected address. JohnWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.