STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Pin Conifguration/Alternate function Map

Posted on February 13, 2013 at 16:04I am fairly new to this, so this might seem like a very basic question. Is there diagram of which GPIO pins can be connected to which alternate functions?For instance something that shows which pins can be used as...

berge472 by Associate II
  • 1656 Views
  • 2 replies
  • 0 kudos

Stm32F4-discovery and USB

Posted on February 12, 2013 at 21:28hi, Can we send data via graphic interface to the stm32F4 via USB ? If it's possible, give me some exemple or what i should do to make USB work. Can we work with USART and USB in the same time ? Can someone help m...

ahmed2399 by Associate II
  • 1348 Views
  • 2 replies
  • 0 kudos

Constant Data at Fixed Flash Address.

Posted on February 12, 2013 at 22:33I have a boot loader that resides in the first flash block of an STM32F4 family processor which is 16K begining at 0x08000000.  I would like the last four byte of the sector at 0x08003ffc to contain constant data ...

STM32F4-Discovery based debugger

Posted on February 12, 2013 at 11:54Hi,There is a short hack on how to make a Cortex debugger from Discovery board at: http://searchingforbit.blogspot.com/2013/02/free-cortex-debugger.html.It is based on free design (not open) without size restricti...

zomirp2 by Associate II
  • 3770 Views
  • 9 replies
  • 0 kudos

STM32-E407 + ARM-USB-TINY + OpenOCD Stack problem

Posted on February 13, 2013 at 14:06Hi, I have successfully programed and debugged my chip many times with toolchain from subject (IAR 6.30.6 + OpenOCD 0.6.1) and everything worked just fine. Then something went wrong. After download IAR threw a wa...

xxmarko by Associate
  • 859 Views
  • 1 replies
  • 0 kudos

STM32F0 peripheral configuration order

Posted on February 13, 2013 at 15:18Is there a specific configuration order for peripherals I need to adhere to so peripherals will function correctly. #stm32f0-peripheral-config

Timer ISR return procedure

Posted on February 11, 2013 at 19:01Hello to everyone.I have just started to study STM32 microcontrolles (using STM32F4 Discovery kit) and can't understand one thing.Test task is simple �? set up Timer 7 to generate 100000 update events per second...

orionhere by Associate II
  • 4328 Views
  • 8 replies
  • 0 kudos

the doubt in M4-Discovery input capture library

Posted on April 19, 2012 at 19:43like this: I don't know why selecting opposite polarity ! /* Select the Opposite Input Polarity */  if (TIM_ICInitStruct->TIM_ICPolarity == TIM_ICPolarity_Rising)  {    icoppositepolarity = TIM_ICPolarity_Falling;  }...

malloc not work on size more then 500 bytes in STM32

Posted on February 12, 2013 at 13:25I try to enter malloc for some area at my programI use IAR 6.4 with STM32F205ZC.first i annunce the buffer pointeruint16_t * ADC3ConvertedValue; and then I call the functionADC3ConvertedValue = (uint16_t*) malloc ...

Barbie by Associate II
  • 1584 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.