2018-03-18 5:11 AM
Hello,
I'm working on a project based on the Nucleo-L432KC board that uses the RTC.I would like to insert a backup battery for the RTC, but I noted that there isn't a VBAT pin where to connect it.
Therefore, cannot a battery backup be used for this board or are there any configurations to be made on it?
Waiting for your feedback
Best RegardsTommaso#rtc #nucleo-l432kc #backup-battery2018-03-18 5:45 AM
Not sure if this pin exists as: '
VBAT pin
is not available on low pin-count packages'2018-03-18 5:45 AM
Look at AN4718 : 'How to design a VBAT system based on
STM32L0/L1 series (with external components)'. The reccomendation should aplly for the L4 too, and the application not should also be extended for the L43 and should also be visible in the L43 product page resources section.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.