2021-03-23 10:18 PM
Hi,
I am using Quad SPI on SHT32H7 and I am looking at examples in STMcube. My question is: Is Chip select for the QSPI handled by the port (inside the silicon) once set or is it my driver function that needs to do it like I had to in regular SPI drivers? I can't find any place in examples all over where Chip select is handled by user functions of even HAL drivers.
2021-03-24 7:04 AM
Hi @RBharol
Do you mean where you can find the CS GPIO Pin configuration?
In the examples you can find it in msp file "stm32h7xx_hal_msp.c". Once the QUADSPI_CS GPIO pin configured, it is automatically managed by the QUADSPI.
Bouraoui
2021-03-24 9:20 AM
The NCS pin is managed by the QSPI peripheral, there are a limited number of choices, and the routing is controlled by the AF association in the GPIO configuration.
2021-03-24 9:24 AM
STM32Cube_FW_H7_V1.5.0\Drivers\BSP\STM32H743I_EVAL\stm32h743i_eval_qspi.h
/* Definition for QSPI clock resources */
#define QSPI_CLK_ENABLE() __HAL_RCC_QSPI_CLK_ENABLE()
#define QSPI_CLK_DISABLE() __HAL_RCC_QSPI_CLK_DISABLE()
#define QSPI_CLK_GPIO_CLK_ENABLE() __HAL_RCC_GPIOB_CLK_ENABLE()
#define QSPI_BK1_CS_GPIO_CLK_ENABLE() __HAL_RCC_GPIOG_CLK_ENABLE()
#define QSPI_BK1_D0_GPIO_CLK_ENABLE() __HAL_RCC_GPIOF_CLK_ENABLE()
#define QSPI_BK1_D1_GPIO_CLK_ENABLE() __HAL_RCC_GPIOF_CLK_ENABLE()
#define QSPI_BK1_D2_GPIO_CLK_ENABLE() __HAL_RCC_GPIOF_CLK_ENABLE()
#define QSPI_BK1_D3_GPIO_CLK_ENABLE() __HAL_RCC_GPIOF_CLK_ENABLE()
#define QSPI_BK2_CS_GPIO_CLK_ENABLE() __HAL_RCC_GPIOC_CLK_ENABLE()
#define QSPI_BK2_D0_GPIO_CLK_ENABLE() __HAL_RCC_GPIOH_CLK_ENABLE()
#define QSPI_BK2_D1_GPIO_CLK_ENABLE() __HAL_RCC_GPIOH_CLK_ENABLE()
#define QSPI_BK2_D2_GPIO_CLK_ENABLE() __HAL_RCC_GPIOG_CLK_ENABLE()
#define QSPI_BK2_D3_GPIO_CLK_ENABLE() __HAL_RCC_GPIOG_CLK_ENABLE()
#define QSPI_FORCE_RESET() __HAL_RCC_QSPI_FORCE_RESET()
#define QSPI_RELEASE_RESET() __HAL_RCC_QSPI_RELEASE_RESET()
/* Definition for QSPI Pins */
#define QSPI_CLK_PIN GPIO_PIN_2
#define QSPI_CLK_GPIO_PORT GPIOB
/* Bank 1 */
#define QSPI_BK1_CS_PIN GPIO_PIN_6
#define QSPI_BK1_CS_GPIO_PORT GPIOG
#define QSPI_BK1_D0_PIN GPIO_PIN_8
#define QSPI_BK1_D0_GPIO_PORT GPIOF
#define QSPI_BK1_D1_PIN GPIO_PIN_9
#define QSPI_BK1_D1_GPIO_PORT GPIOF
#define QSPI_BK1_D2_PIN GPIO_PIN_7
#define QSPI_BK1_D2_GPIO_PORT GPIOF
#define QSPI_BK1_D3_PIN GPIO_PIN_6
#define QSPI_BK1_D3_GPIO_PORT GPIOF
/* Bank 2 */
#define QSPI_BK2_CS_PIN GPIO_PIN_11
#define QSPI_BK2_CS_GPIO_PORT GPIOC
#define QSPI_BK2_D0_PIN GPIO_PIN_2
#define QSPI_BK2_D0_GPIO_PORT GPIOH
#define QSPI_BK2_D1_PIN GPIO_PIN_3
#define QSPI_BK2_D1_GPIO_PORT GPIOH
#define QSPI_BK2_D2_PIN GPIO_PIN_9
#define QSPI_BK2_D2_GPIO_PORT GPIOG
#define QSPI_BK2_D3_PIN GPIO_PIN_14
#define QSPI_BK2_D3_GPIO_PORT GPIOG/**
* @brief QSPI MSP Initialization
* This function configures the hardware resources used in this example:
* - Peripheral's clock enable
* - Peripheral's GPIO Configuration
* - NVIC configuration for QSPI interrupt
* @retval None
*/
__weak void BSP_QSPI_MspInit(QSPI_HandleTypeDef *hqspi, void *Params)
{
GPIO_InitTypeDef gpio_init_structure;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable the QuadSPI memory interface clock */
QSPI_CLK_ENABLE();
/* Reset the QuadSPI memory interface */
QSPI_FORCE_RESET();
QSPI_RELEASE_RESET();
/* Enable GPIO clocks */
QSPI_CLK_GPIO_CLK_ENABLE();
QSPI_BK1_CS_GPIO_CLK_ENABLE();
QSPI_BK1_D0_GPIO_CLK_ENABLE();
QSPI_BK1_D1_GPIO_CLK_ENABLE();
QSPI_BK1_D2_GPIO_CLK_ENABLE();
QSPI_BK1_D3_GPIO_CLK_ENABLE();
QSPI_BK2_CS_GPIO_CLK_ENABLE();
QSPI_BK2_D0_GPIO_CLK_ENABLE();
QSPI_BK2_D1_GPIO_CLK_ENABLE();
QSPI_BK2_D2_GPIO_CLK_ENABLE();
QSPI_BK2_D3_GPIO_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* QSPI CLK GPIO pin configuration */
gpio_init_structure.Pin = QSPI_CLK_PIN;
gpio_init_structure.Mode = GPIO_MODE_AF_PP;
gpio_init_structure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
gpio_init_structure.Pull = GPIO_NOPULL;
gpio_init_structure.Alternate = GPIO_AF9_QUADSPI;
HAL_GPIO_Init(QSPI_CLK_GPIO_PORT, &gpio_init_structure);
/* QSPI CS GPIO pin configuration */
gpio_init_structure.Pin = QSPI_BK1_CS_PIN;
gpio_init_structure.Pull = GPIO_PULLUP;
gpio_init_structure.Alternate = GPIO_AF10_QUADSPI;
HAL_GPIO_Init(QSPI_BK1_CS_GPIO_PORT, &gpio_init_structure);
gpio_init_structure.Pin = QSPI_BK2_CS_PIN;
gpio_init_structure.Mode = GPIO_MODE_AF_PP;
gpio_init_structure.Pull = GPIO_PULLUP;
gpio_init_structure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
gpio_init_structure.Alternate = GPIO_AF9_QUADSPI;
HAL_GPIO_Init(QSPI_BK2_CS_GPIO_PORT, &gpio_init_structure);
...
2021-03-24 9:48 AM
Thanks, Bouraoui,
>> it is automatically managed by the QUADSPI.
That answers my question. Does it mean this limits the number of devices we can have on QSPI?
2021-03-24 9:50 AM
Thanks.
What do Bank 1 ann Bank 2 signify?
2021-03-24 10:40 AM
The H7 supports two QSPI devices. either as distinct devices, or paired to improve the bandwidth.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.