2026-01-04 1:54 AM - edited 2026-01-04 2:10 AM
Hi I have a question that blocked me for several days, Hopefully someone can help, thanks a lot.
1:MCU:STM32G0B0CET6,Develop tool:STM32CubeIDE
2:I wanna have a test for OTA ,so i create a bootloader project and app project
3:Flash segmentation:
1)Bootloader(32KB),0x08000000~0x08007FFF
APP(240K):0x08008000~0x08047FFF
APP BAK(236K):0x08048000~0x08079FFF
INFO(8K):0x0807A000~x0807FFFF
4:In Bootloader ,try to jump to APP(0x08008000):
5:Attached the source code (bootloader and app) and hex file(in debug directory)
6:Modifed "ld" file in bootloader project and app project, and I confirm the stack address in 0x08008000 and reset_handler in 0x08008004 is correct.
And have set vector in main entry(first line in main()):SCB->VTOR = FLASH_BASE | 0x8000;
7:If i use stm32CubeProgrammmer and STM32CubeIDE to start ,app will be run ,But app can not run via bootloader software jump.
bootloader jump slide:
void RunUserCode( void )
{
uint32_t* ucaddr;
// if( ( ( *( uint32_t* )ROM_APP_VECT_START_ADDR ) & 0x2FFC0000 ) == 0x20000000 )
if( ( *( uint32_t* )APP1ADDR ) == 0x20023FF8)
{
HAL_DeInit();//DeInit The Peripherals Used By The Bootloader
//Rocky report fault shield first __set_FAULTMASK( 1 );
__disable_irq();
__set_MSP( *( __IO uint32_t* )APP1ADDR ); // Get top of stack address and initialize SP
__set_PSP( *( __IO uint32_t* )APP1ADDR );
__set_CONTROL( 0 );
ucaddr = ( uint32_t* )( ROM_APP_VECT_RESET_ADDR ); // Get APP Reset Handler address
( *( ( void( * )( void ) )( *ucaddr ) ) )(); // Let's Jump!
}
}app vector set:
int main(void)
{
/* USER CODE BEGIN 1 */
/* 第一步:强制设置向量表偏移,优先级最高 */
//SCB->VTOR = 0x08008000; // 必须放在最前面!
SCB->VTOR = FLASH_BASE | 0x8000;
setMainState(BOOT,3);
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();bootloader ld slice: :
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 144K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 32K
}
/* Sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
APP ld Slice:
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = 0x20023FF8;/*8 bytes alignment*/
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 144K
FLASH (rx) : ORIGIN = 0x08008000, LENGTH = 240K
}
/* Sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASHflash readback screen shot for boot and app:
Solved! Go to Solution.
2026-01-14 3:20 AM
Just make sure that the .noinit is placed in the script AFTER .bss, not between .data and .bss. :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.