2019-02-11 2:44 PM
I want to have one STM32F730 using a crystal on OSCIN and OSCOUT, and then slave 7 other STM32F730s to the same clock. But if I connect OSCIN of these other 7 to OSCOUT of processor 1 I assume it will load that pin with too much capacitance. I can't see a way of getting a buffered clock out at the crystal frequency fHSE to drive the other processors so do I have to add an external buffer ?
2019-02-11 3:14 PM
Look at the schematics for any of the Nucleo boards. They use one STM32 as a debugger with a crystal attached and feed the main STM32 clock in.
I don't remember the details, but they're all in the schematics.
2019-02-11 3:34 PM
Well not all Nucleo board it would seem, but eventually found one as you described. The MCO function isn't described in the STM32F730 datasheet but I found the details in another STM32 device. Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.