STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN communication using STMF103

I am new with CAN bus implementation,can somebody point me in right direction?Example project would be the best.Thank youAlexei

ATikh by Associate II
  • 1952 Views
  • 4 replies
  • 0 kudos

Resolved! Stm32f4: Program Erased on Power Cycle -- SOLVED

First post on the forum...I’m currently programming a custom PCB with an Stm32f446ret6 for an uC. Using an SWD interface and System Workbench the program uploads fine. However when I disconnect the board, and then hook it up to an external P.S. the p...

dlepe by Associate II
  • 5781 Views
  • 6 replies
  • 0 kudos

Wrong Data send after correct Addr with I2C

Hi,I'm still having trouble with my I2C communication. I'm using the Bus as Master, at the moment without any Slave. After sending the Device Addr, which is transmitted correctly to the ouput (checked with logic analyser) I send data which is then pu...

0690X000006DTALQA4.png 0690X000006DTAGQA4.png
uli stone by Associate II
  • 3226 Views
  • 6 replies
  • 0 kudos

Same Library file working on stm32f7 but not on stm32f4

I am stuck with a really weird issue while using time of flight sensor VL53L0x - 200 cm andVL6180x - 60 cm. I have two st boards, STM32F446 Nucleo and STM32F767 Nucleo. I have written the libraries for both the time of flight sensors on STM32F767 Nuc...

STM32F334 - using HRTIM for triggering ADC sampling

Hello,we are using the HRTIM (Channel A) of the STM32F334 to trigger the ADC.The data of the ADC is written to an uint16[3] array by using the DMA.We disabled the IRQ for the specific DMA channel as the ADC value is used by the main program with lowe...

s m by Associate III
  • 1533 Views
  • 0 replies
  • 0 kudos

output from STM32F4 board to the speaker

 I am using STM32F407 board with cortex-m4 and Wolfson pi audio extension card. I am using Keil micro vision 5. I Want to generate white Gaussian noise signal using the code(which I have to write) and I want to pass that output to the speaker. I went...

rrach by Associate II
  • 1570 Views
  • 2 replies
  • 0 kudos

Help, what is going on ???

Hi if anyone can help it will be very much appreciatedYet another strange issueso I have my stlink v2 debugger set up with Rowley crossstudioeverything works fine when debugging and running my code from the ide on my nucleo st32f446RE board, yet whe...

JHERI by Senior
  • 3677 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.