2019-05-31 9:20 PM
Hello,
I have an application in which waveform is generated (DAC1, updated triggered with T6), data is acquired (ADC1_INP2 and ADC2_INP3, dual simultaneous mode, triggered with T3), T2 is used to control the waveform, ADC_DMA in circular mode is employed. I have options of using either the internal PHY or external PHY (Waveshare USB3300) for transferring data back to the host PC. The data transfer takes place at DMAHalfComplete and DMAComplete interrupts, respectively. With the internal PHY the program runs ok but I want to go faster up to at least 2MHz of ADC sampling rate and transfer chunks of data back to the host PC. But I have confronted problem with the external PHY. So far I can make the software run with a few wonders:
Any input would be appreciated!
Many thanks,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.