2017-07-30 1:48 AM
Hi,
I set two F303VC Discovery boards with the same configuration using cubeMx: they have same clock on apb2 bus and time segment 1 and 2 and RJW are both the same.
One is programmed as a receiver and the other as a transmitter.there is no of communication .
I tested this setting in loopback mode and the test was succesful.
Should I configure clock and bit time parameters in a particular way? Is the problem linked to the wiring? I connected only CANtx to CANtx and CANrx to CANrx (this pin's names are strange because i know that CAN is a differential protocol, so there must be CANH and CANL).
Thanks a lot for any answer.
#can-canopen #can-bus-stm32f303 #can2017-07-30 7:10 AM
>>I connected only CANtx to CANtx and CANrx to CANrx (this pin's names are strange because i know that CAN is a differential protocol, so there must be CANH and CANL).
Doesn't work like that, you need a transceiver or diode circuit to construct the bus.
See circuit 60% down this thread using SN65VD230
https://community.st.com/0D50X00009XkiDZSAZ
2017-07-30 7:25 AM
2017-07-31 8:35 AM
Hi Marco,
In this post you could find information that could help to you:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.