2010-05-13 4:36 AM
Can Bus between 9 card
2011-05-17 4:50 AM
I am hoping that every slave is using the same CAN code to send or receive CAN packet if this is the case just make sure that all slave devices dont send at the same time,use Tx FIFO and also some hw/sw buffer at the Master Rx side.
Use filtering so that other slave devices dont receive unwanted data.2011-05-17 4:50 AM
Hi, avr-smart
First, thx for your reply. Yes, All of node are common. I know, the filters chose slaves but How and where can I define filters for all slaves in program. At first of program(Following?) or while sending? Can_Setup(); Can_Filter(CPU_ID,filter_no0); Can_Filter(Slave_ID1,filter_no1); Can_Filter(Slave_ID2,filter_no2); Can_Filter(Slave_ID3,filter_no3); Can_Filter(Slave_ID4,filter_no4); Can_Filter(Slave_ID5,filter_no5); Can_Filter(Slave_ID6,filter_no6); Can_Filter(Slave_ID7,filter_no7); thx again2011-05-17 4:50 AM
Thx for your reply
I solved my problem and the comunication.2011-05-17 4:50 AM
Ii am not sure about your application, are slave devices talking with each other or all sending data to master.
If they are not talking to each other just sending data to master then filtering is most useful based on CAN packet id or some range for receiving CAN packets.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.