2010-05-12 3:44 PM
SPI2
2011-05-17 4:50 AM
/* Defines for the SPI and GPIO pins used to drive the SPI Flash */
#define SPI_FLASH SPI2 #define SPI_FLASH_CLK RCC_APB1Periph_SPI2 #define SPI_FLASH_GPIO GPIOB #define SPI_FLASH_GPIO_CLK RCC_APB1Periph_SPI2 #define SPI_FLASH_CS_GPIO_CLK RCC_APB2Periph_GPIOB #define SPI_FLASH_CS GPIO_Pin_12 #define SPI_FLASH_PIN_SCK GPIO_Pin_13 #define SPI_FLASH_PIN_MISO GPIO_Pin_14 #define SPI_FLASH_PIN_MOSI GPIO_Pin_15 #define SPI_FLASH_CS_GPIO GPIOB /******************************************************************************* * Function Name : SPI_FRAM_Init * Description : Function to initialize SPI * Return : None *******************************************************************************/ VOID SPI_FRAM_Init(VOID) { SPI_InitTypeDef SPI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure;/* Enable SPI and GPIO clocks */
RCC_APB1PeriphClockCmd(SPI_FLASH_CLK | SPI_FLASH_GPIO_CLK | SPI_FLASH_CS_GPIO_CLK, ENABLE);/* Configure SPI pins: SCK, MISO and MOSI */
GPIO_InitStructure.GPIO_Pin = SPI_FLASH_PIN_SCK | SPI_FLASH_PIN_MISO | SPI_FLASH_PIN_MOSI; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(SPI_FLASH_GPIO, &GPIO_InitStructure);/* Configure I/O for Flash Chip select */
GPIO_InitStructure.GPIO_Pin = SPI_FLASH_CS; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(SPI_FLASH_CS_GPIO, &GPIO_InitStructure);/* Deselect the FLASH: Chip Select high */
SPI_FLASH_CS_HIGH();/* SPI configuration */
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2; /* PCLK1 = HCLK/4 72/4=18= 18/2= 9Mhz*/ SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI_FLASH, &SPI_InitStructure);/* Enable the SPI */
SPI_Cmd(SPI_FLASH, ENABLE); }2011-05-17 4:50 AM
I am having a problem setting the RCC_APB2Periph_SPI2 because there is no define for the register value
Because it is on the APB1 bus, not APB2RCC_APB1Periph_SPI22011-05-17 4:50 AM
Thanks guys. I spotted that about 20 minutes after posting .... I feel like such a muppet, I must stop working late as it all blurs together
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.