2010-05-14 3:48 AM
Remapping Cortex STM32 GPIO
2011-05-17 4:50 AM
I don't think remapping PA8 is possible. Look in your device reference manual for the Pin Definitions Table. In the 105 device it is Table 5. For at least the 105 device, there is no remapping available for PA8.
Cheers, Hal2011-05-17 4:50 AM
Hi,
TIM1_CH1 can be remapped only on PE9 pin (full remap) (for 100/144 pin packages): register AFIO_MAPR:Bits 7:6 TIM1_REMAP[1:0]: TIM1 remappingThese bits are set and cleared by software. They control the mapping of TIM2 channels 1 to
4, 1N to 3N, external trigger (ETR) and Break input (BKIN) on the GPIO ports.
00: No remap (ETR/PA12, CH1/PA8, CH2/PA9, CH3/PA10, CH4/PA11, BKIN/PB12,
CH1N/PB13, CH2N/PB14, CH3N/PB15)
01: Partial remap (ETR/PA12, CH1/PA8, CH2/PA9, CH3/PA10, CH4/PA11, BKIN/PA6,
CH1N/PA7, CH2N/PB0, CH3N/PB1)
10: not used
11: Full remap (ETR/PE7, CH1/PE9, CH2/PE11, CH3/PE13, CH4/PE14, BKIN/PE15,
CH1N/PE8, CH2N/PE10, CH3N/PE12) Cheers.
2011-05-17 4:50 AM
It is not gpio pins that are remapped, it is peripherals.
If you want PWM output on PB1, then use timer 3 channel 4. No remapping is required to do this.2011-05-17 4:50 AM
Thanks, I will try using TIM4
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.