2016-01-25 7:30 AM
Hi!
I use the example CANdata from Keil.STM32F1xx_DFP.2.5.0 pack and can not get CAN channel 2 to transmit any messages. The example uses external loopback. I dont need to show or use the LCD due to I have a CAN logger that can receive the messages sent on CAN. Channel 1 works but no messages are sending to channel 2. &sharpdefine CAN_CONTROLLER 1 // CAN Is is possible to just change two 2 above to try channel 2 or do I have to change anything else? My setup is CAN ch 1 to Saleae logger ch 2 CAN ch 2 to saleae logger ch 2 I use ground even if I dont have to as I understand. I have the STM32F107VCT6 microcontroller and board MCBSTM32C (http://www.keil.com/boards2/keil/mcbstm32c/) using Keil. I Attached original example. #can #canbus #stm32f12016-01-25 8:27 AM
Hi Friendship,
With STM32F107 device, you should be using the STM32F1 software pack (Keil.STM32F1xx_DFP.2.0.0.pack).If you still have an issue, I suggest you submit your problem in Keil's forum.I recommend you also to have a look to CAN examples available in our firmware packages.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-01-25 9:53 AM
2016-01-25 10:21 AM
No, ST has SPL and HAL/Cube firmware libraries that you can download from this site. ST and Keil provide their own code, being unrelated companies. In uV4 Keil provided third-party libraries, but was usually lagging the release schedule.
The F1 uses an older CAN IP design, you are best to start off with code/examples tailored to what you are using. The may be many commonalities, but it's the differences that will bite you. CAN2 is a slave device on STM32 implementation, it uses a lot of the CAN1 peripheral resources they have in common, and CAN1 must be up and functional.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.