2016-01-25 10:50 AM
Hi,
I have an issue with the STM32F429 (Discovery board with 8 MHz crystal).I created a Keil project (software pack based) and added the following SW packs:CMIS: CoreCMIS: DSPDevice: StartupThen I added the following main file:#include ''stdio.h''#include ''stm32f4xx.h''// PLL register values#define PLL_MASK 0x80BC8000 // PLL register mask#define PLLM_VAL 4 // PLL division factor#define PLLN_VAL 180 // PLL multiplication factor#define PLLP_VAL 0 // 0: div by 2#define PLLSRC_VAL 1 // HSE is source to PLL#define PLLQ_VAL 2 // PLLQ: not used#define PLLR_VAL 2 // PLLRint main(void){ RCC->CFGR = (RCC->CFGR & 0xFFFFFF0F); // AHB prescaler : 1 RCC->CFGR = (RCC->CFGR & 0xFFFFE3FF) | 0x1400; // APB1 prescaler: 4 RCC->CFGR = (RCC->CFGR & 0xFFFF1FFF) | 0x8000; // APB2 prescaler: 2 RCC->CR |= 0x10000; while((RCC->CR & 0x20000) != 0x20000){ // wait for HSE ready } RCC->PLLCFGR = (RCC->PLLCFGR & PLL_MASK) | ((PLLR_VAL << 28) | (PLLQ_VAL << 24) | (PLLSRC_VAL << 22) | (PLLP_VAL << 16) | (PLLN_VAL << 6) | PLLM_VAL); // Setup PLL RCC->CR |= 0x1000000; // Main PLL: ON while((RCC->CR & 0x2000000) != 0x2000000){ // wait for PLL ready } RCC->CFGR = (RCC->CFGR & 0xFFFFFFFC) | 0x02; // PLL_P is selected as system clock while((RCC->CFGR & 0x08) != 0x08){ // wait PLL_P to be used as system clock } RCC->CR = RCC->CR & 0xFFFFFFFE; // HSI oscillator disable while(1){ } }But the CPU crashes after setting up the clocks. Any ideas?Thank you.2016-01-25 10:58 AM
Flash wait states?
2016-01-25 11:26 AM
That was it. Thank you!
I spent hours trying to figure this out!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.