2013-09-03 2:23 AM
Hi,
I've been experimenting on USB devices on STM32F4 discovery board. I have a small issue.From the PC I send multiple messages (bulk_writes) to the USB, and I call 'dcd_ep_tx' within the Data_out function which invokes upon transfer complete interrupt on OUT packets. The issue is when I do this and later when I read the same endpoint, I can receive around 4~7 packets which I have previously sent to the device. I still could not find the source for this behavior. I'm using the cdc example as the foundation in this application.Is this due to some sort of a FIFO? If so where is it implemented? My TX1 FIFO size is 128.I hope the question is clear. Thank you in advance. #stm32f42013-09-05 11:53 PM
Anyone???
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.