Debug with GDB - Symbols names
Posted on September 06, 2013 at 17:58Hi,It is possible to use symbols names in gdb? per example:p GPIOA->BSRR instead of: p *(0x40020000+0x18) ?Thanks :)
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on September 06, 2013 at 17:58Hi,It is possible to use symbols names in gdb? per example:p GPIOA->BSRR instead of: p *(0x40020000+0x18) ?Thanks :)
Posted on September 06, 2013 at 14:32I'm trying to calibrate the difference of 512Hz at the out where PC13 possess 511.936Hz which causes about 10 seconds per day delay in the RTC. I'm making the form below, I wonder where I'm going wrong, not beca...
Posted on September 06, 2013 at 08:37I want to store part of my code on an SD card and execute it whenever a certain event occurs. I've already figured out how to interface with an SD card so the problem now it getting the machine code into RAM and ...
Posted on September 05, 2013 at 23:34Hi, I work with STM32F100RB chip and i got a little problem with editting registers of some peripheral. I got a problem with edit DMA registers. Even if I use code from DMA example in my project and build it, the...
Posted on September 01, 2013 at 19:04i'm tryng to simply get 50Hz PWM out of 4 pin, timer used is TIM4, pins are D10, D11, D12 and D13. but i get a fixed HIGH.. code: int init_pwm2(int pwm_freq) { GPIO_InitTypeDef GPIO_InitStruct; /*Enable ...
Posted on September 04, 2013 at 17:19Hi there, If PortD is originally configured as input and then the following code is executed, how long will it take 0x5AA5 to appear on portD after the ->CRL assignment completes? Can't seem to find this in t...
Posted on September 05, 2013 at 17:43Hi guys, I've got a stm32f10zg eval board and am trying to set up a timer on it to generate an interrupt at a frequency of 8MHz. I've got the PLL set up a a x9 so that the timer is getting a 72 MHz input clock. I...
Posted on September 03, 2013 at 11:23Hi,I've been experimenting on USB devices on STM32F4 discovery board. I have a small issue.From the PC I send multiple messages (bulk_writes) to the USB, and I call 'dcd_ep_tx' within the Data_out function which ...
Posted on September 06, 2013 at 03:54The code I'm porting use the __nop() function the delay but I don't have that function on F1, should I use the systick instead?https://github.com/metropt/STM32StepperDriver/blob/master/Source/main.c#L28thanks :)
Posted on September 06, 2013 at 00:09 Hi, I'm porting a code from F4 to F3 and one of the erros I'm getting is: stm32f_stpdrv.c: In function 'TIM3_IRQHandler': stm32f_stpdrv.c:192:20: error: 'GPIO_TypeDef' has no member named 'BSRRH' s...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.