2023-01-23 5:20 PM
Hello all....
Ok....not sure what i am missing here but this fails miserably....
The compiler hates when I try and assign test =
The return function works fine, I have made the return variable static so as not to lose the scope....test is an array so I expect test is the same as me doing &test[0]...What am I missing here?
uint8_t test[6];
for (uint8_t k = 0; k < NO_ADC_CH; k++)
{
test = hex2Ascii(&stream[k]);
test[4] = '\r';
test[5] = '\n'; //new line
HAL_UART_Transmit_IT(&huart2, test, sizeof(test));
}
char*hex2Ascii(uint16_t *val)
{
unsigned char d;
static char buff[4];
buff[0] = (char)((d = (*val >> 12)) > 9 ? ('A' + d - 10) : ('0' + d));
buff[1] = (char)((d = ((*val >> 8) & 0xf)) > 9 ? ('A' + d - 10) : ('0' + d));
buff[2] = (char)((d = ((*val >> 4) & 0xf)) > 9 ? ('A' + d - 10) : ('0' + d));
buff[3] = (char)((d = (*val & 0xf)) > 9 ? ('A' + d - 10) : ('0' + d));
return buff;
}
Solved! Go to Solution.
2023-01-25 1:43 PM
By definition a[b] is the same as *(a + b), which is the same as *(b + a), which is the same as b[a]. That's just C.
2023-01-26 12:06 AM
Live and learn, as they say ))
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.