2012-06-18 4:32 AM
I am using the STM32F4 family with Atollic TrueStudio and would like to use the CMIS DSP_Lib for my application. The STM32F4xx_DSP_StdPeriph_Lib_V1.0.1 directory as provided by ST does not appear to have pre-built GCC libraries.
There is an ARM directory with files such as arm_cortexM4lf_math.lib but the GCC directory is empty. Under the source directory there is a GCC folder with uvproj files but I am not using Kiel. Any advice for building GCC binaries view Atollic TrueStudio would be greatly appreciated. The libraries Attolic provides are of the lib*.a variety. John2012-06-18 8:14 AM
Create a project, and rebuild using the tools of your choice.
You are supposedly able to build this with Keil (Evaluation) using GNU/GCC, presumably Code Sourcery. This proved to be more of a battle than I cared to fight, so I just built it with Yagarto 4.6.2, using a batch file. Attached is the build from DSP V1.0.0, would need to download the newer DSP Library. ________________ Attachments : libarm_cortexM4lf_math.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtTd&d=%2Fa%2F0X0000000aQV%2FBaP1PKa4r_ZhNO07CVPH4w7aFclBosGyyGh686kkUvw&asPdf=false2012-06-18 9:18 AM
Attached libraries built from V1.0.1
________________ Attachments : libarm_cortexM4_math_V1.0.1.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtQ2&d=%2Fa%2F0X0000000aPj%2FV53blwXRlopjTdw4KzoRmRZ8cUrgj37EA9K3oTPO83k&asPdf=false2012-06-18 11:42 AM
Thank you. I will try the attachment. Hopefully it is compatible with the discovery board.
John2012-06-18 11:55 AM
Hopefully it is compatible with the discovery board.
I would imagine that it's board agnostic, it's all about the CPU. Make sure you enable/initialize the FPU in your startup code.2014-01-10 2:59 PM
From: clive1
Posted: Monday, June 18, 2012 5:14 PMSubject: Building CMSIS DSP_LIB for GCCCreate a project, and rebuild using the tools of your choice.
You are supposedly able to build this with Keil (Evaluation) using GNU/GCC, presumably Code Sourcery. This proved to be more of a battle than I cared to fight, so I just built it with Yagarto 4.6.2, using a batch file.Attached is the build from DSP V1.0.0, would need to download the newer DSP Library.2014-01-11 5:11 PM
Was there a question there somewhere?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.