STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Normal Transmit fails but Loopback works

Posted on January 13, 2014 at 14:46 Ok, I got the LoopBack to work. But, now I can not get it to work in Normal mode. I have it running on (2) Stm32f103C8 chips. I have a mcp2551 attached to each board, and the mcp2551 chips cross connected. But ...

Falling edge detection by hardware but without Interrupt

Posted on January 11, 2014 at 13:49Hi all,I want to detect a falling edge on external pinn let's say PD13 by hardware but without using the interrupt capability (using EXTI + NVIC).At first time I thought it is possible to do that using EXTI only by...

USART receiving with interrupts doesn't work

Posted on January 06, 2014 at 10:15Hi all,I'm trying to receive char using USART through interrupts but it seems doesn't work (it doesn't receive the interrupt when I prompt a char in the terminal).I use USB To RS232 TTL UART PL2303HX for connect st...

VREFINT Measurement Issue in STM32L

Posted on January 11, 2014 at 17:28HelloI am trying to implement indirect voltage measurement in a battery operated application.Our MCU supports VREF+ and VREF+ is derived from the battery voltage. Therefore - VREFINT must be used to extract VREF+.T...

gilt by Associate
  • 1085 Views
  • 1 replies
  • 0 kudos

ADC in regular dual simultaneous mode in stm32f4 discovery

Posted on January 11, 2014 at 19:31I've a small query about programming ADC in regular dual simultaneous mode. I'm using stmf4 discovery board.Though I've configured ADC1 channel 11(PC1) and ADC2 channel 12(PC2) in this mode using dma. But I've to c...

sen by Associate II
  • 2738 Views
  • 3 replies
  • 0 kudos

Trouble using STM32F4's CRC on 8 bit array

Posted on January 12, 2014 at 01:29I am using a STM32F4's internal CRC peripheralMy test sample data works against the code available at http://www.opensource.apple.com/source/xnu/xnu-1456.1.26/bsd/libkern/crc32.cSample data is { 0xA1, 0x11, 0xC0, 0...

STM32 USART debugging

Posted on January 11, 2014 at 12:51Hello everyone,I would be very gratefull if you help me with this or give me some idea. I have problem with STM32100RB USART module. It uses Cortex M3 and I am developing in Keil uvision.The USART uses hardware flo...

empnik by Associate
  • 1746 Views
  • 2 replies
  • 0 kudos

Building CMSIS DSP_LIB for GCC

Posted on June 18, 2012 at 13:32I am using the STM32F4 family with Atollic TrueStudio and would like to use the CMIS DSP_Lib for my application.    The STM32F4xx_DSP_StdPeriph_Lib_V1.0.1 directory as provided by ST does not appear to have pre-built ...

jdsotack by Associate II
  • 3020 Views
  • 6 replies
  • 0 kudos

Minimum circuit for bare STM32 F2 lqfp64?

Posted on January 10, 2014 at 23:38I don't have one of the discovery boards (I know, I know ;), just a small stack of F205 chips. I'm breadboarding one up so I can get a handle around it, and having trouble identifying the minimum circuit needed for...

skeezix by Associate II
  • 1779 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.