2013-04-25 3:11 AM
Hello ;
In the recording example in teh discovery board we have this code :if(Data_Status==1)
{
Data_Status=0;
/* Switch the buffers*/
if (Switch ==1)
{
pAudioRecBuf = RecBuf;
writebuffer = RecBuf1;
WaveCounter += 32;
Switch = 0;
}
else
{
pAudioRecBuf = RecBuf1;
writebuffer = RecBuf;
WaveCounter += 32;
Switch = 1;
}
for (counter=0; counter<16; counter++)
{
if (buf_idx< RAM_BUFFER_SIZE)
{
/* Store Data in RAM buffer */
RAM_Buf[buf_idx++]= *(writebuffer + counter);
if (buf_idx1 == RAM_BUFFER_SIZE)
{
buf_idx1 = 0;
/* Write the stored data in the RAm to the USB Key */
f_write (&file, (uint16_t*)RAM_Buf1, RAM_BUFFER_SIZE*2 , (void *)&bytesWritten);
}
}
else if (buf_idx1< RAM_BUFFER_SIZE)
{
/* Store Data in RAM buffer */
RAM_Buf1[buf_idx1++]= *(writebuffer + counter);
if (buf_idx == RAM_BUFFER_SIZE)
{
buf_idx = 0;
/* Write the stored data in the RAM to the USB Key */
f_write (&file, (uint16_t*)RAM_Buf, RAM_BUFFER_SIZE*2 , (void *)&bytesWritten);
}
}
}
}
} I believe
RAM_Buf1 stores the wrong data and all the time
RAM_Buf only been used , Please check it
Regards
Esat
2013-06-20 9:31 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.