2013-06-19 5:17 PM
2013-06-20 7:53 AM
Remapping the ADC pins to AN mode should do it. But I won't wade through your register code to see if something else is wrong.
Cheers, Hal2013-06-20 9:22 AM
Believe Hal makes very valid point, ''I won't wade through your register code to see if something else is wrong.''
Might your post (and that of others) benefit by your reducing and confining the code presented to just the essence? (as the code block extends - review effort increases - likelihood of response thus decreases...) In your case - single ADC channel presentation would greatly shrink/simplify. (you can easily then generalize single channel into multiple) Further - should standard, vendor API code be available - that is most always preferable to ''register code'' - which is not likely to be ''intuitive'' to code reviewers... Suggest that you employ vendor API code for single channel - note results. Review of that code likely to reveal registers and logic ''in play'' - and then better enable your later success w/register code - if that is even necessary...2013-06-20 9:36 AM
Might your post (and that of others) benefit by your reducing and confining the code presented to just the essence?
Totally agree... Also I suggest to use ''Format code block'' feature for codes. This makes them easily readable. -Mayla-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.