2024-04-29 2:13 AM - last edited on 2024-04-29 2:40 AM by mƎALLEm
Hello,
I am currently fiddling around with a STM32G491 in bare metal. I wanted to test the write protection. So I executed following code
FLASH->KEYR = FLASH_KEY1;
FLASH->KEYR = FLASH_KEY2;
while(FLASH->CR&bit31); // wait for unlock
FLASH->OPTKEYR = FLASH_OPTKEY1;
FLASH->OPTKEYR = FLASH_OPTKEY2;
while(FLASH->CR&bit30); // wait for option unlock
//#define PROTECT(start, end) FLASH->WRP1AR = (((start>>11)&0xFF)|(((end>>11)&0xFF)<<16))
PROTECT(0x5000, 0x6000);
FLASH->CR |= bit17; // option start
while(FLASH->CR&bit17); // wait for option done
FLASH->CR |= bit27; // option load
while(FLASH->CR&bit27); // wait for option reload done
FLASH->CR |= bit30; // lock option
FLASH->CR |= bit31; // lock
Just to note my code worked fine (except the locking) until I added line 12. It seems the OB_LAUNCH bit is never reset to 0.
The problem is now that I can not reach my device any more. I am connected through SWD via STlinkV2 with a hardware reset connectd. But none of the connection methods works any more using STProg or STCubeIDE. Not even connect under reset works. How can that be? Is there anything I can do to erase it?
Edit: the error I get is
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
Solved! Go to Solution.
2024-04-29 2:26 AM
Is it stuck running this code again?
Try pulling BOOT0 High?
2024-04-29 2:26 AM
Is it stuck running this code again?
Try pulling BOOT0 High?
2024-04-29 2:38 AM
Thanks for the reply. But it didnt do anything pulling boot0 to high. Also not when trying to connect while Boot0 is high.
I hooked up a logic analyzer to the reset line. I see ~3,8ms high pulse every ~140ms. The reset is low otherwise. Also when the STLink is not connected these pulses are there.
This pattern does not change if the STlink is connected and I try to connect under reset. Shouldn't the STlink pull the reset low in order to connect?
2024-04-29 2:44 AM
Working again. Seems fiddeling with the Boot0 pin high and low while connecting somehow anabled STprog to connect.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.