2017-08-25 5:37 PM
Hi,
recently I started my adventure with STM32F103C8T6. I had some experience with programming on other boards e.g STM32F3 Discovery but I came accross a problem with external interruptions. I am using EclipseStm as IDE, where my trouble making board was not defined as default (I have to do it myself). I have to point out that I did some research and i did not found any solution.
Also, I have to point out that I have no problems with other interruptions e.g TIMx and SysClock on this board.
Basing on my knowledge from Discovery board I have created this simple code:
&sharpinclude <stdbool.h>&sharpinclude 'stm32f10x.h'&sharpdefine DIOD GPIO_Pin_3
&sharpdefine INT GPIO_Pin_11&sharpdefine INT_SRC GPIO_PinSource11void init() {RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);//initializing blinking diod
GPIO_InitTypeDef GPIOinit;
GPIOinit.GPIO_Pin = DIOD; GPIOinit.GPIO_Mode = GPIO_Mode_Out_PP; GPIOinit.GPIO_Speed = GPIO_Speed_2MHz; GPIO_Init(GPIOA, &GPIOinit);//initializing input pin
GPIOinit.GPIO_Pin = INT; GPIOinit.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOB, &GPIOinit);
//initializing exti
GPIO_EXTILineConfig(GPIO_PortSourceGPIOB, INT_SRC); EXTI_InitTypeDef EXTIinit; EXTIinit.EXTI_Line = EXTI_Line11; EXTIinit.EXTI_LineCmd = ENABLE; EXTIinit.EXTI_Mode = EXTI_Mode_Interrupt; EXTIinit.EXTI_Trigger = EXTI_Trigger_Rising_Falling; EXTI_Init(&EXTIinit);//initializing handler
NVIC_EnableIRQ(EXTI15_10_IRQn); NVIC_SetPriorityGrouping(NVIC_PriorityGroup_2); NVIC_InitTypeDef NVICinit; NVICinit.NVIC_IRQChannel = EXTI15_10_IRQn; NVICinit.NVIC_IRQChannelCmd = ENABLE; NVICinit.NVIC_IRQChannelPreemptionPriority=2; NVICinit.NVIC_IRQChannelSubPriority=2; NVIC_Init(&NVICinit);}void EXTI15_10_IRQHandler() {
static bool flag = false;
if(EXTI_GetITStatus(INT_SRC) != RESET) {
flag ? GPIO_SetBits(GPIOC, DIOD) : GPIO_ResetBits(GPIOC, DIOD); flag = !flag; }EXTI_ClearITPendingBit(INT_SRC);
}int main(void)
{ init();while(1);
}I have figured out that (in my case) there is no EXTI15_10_IRQHandler function call. I cannot find even its declaration while searching peripherial library files (in F3 board there is occurence).My question is there something wrong with my library that I do not have some functions? Or Maybe I am doing something wront with initialization? Can someone explain this strange behavoir?
#interrupts #stm32f103c8t6We’re moving the ST Community to a new platform to give you a better and more reliable community experience.