2025-11-04 10:58 PM
Hi,I want to use STM32G431CB or STM32F411CEU6 to measure the time precisely.I need to know the external interrupt response time of GPIO,but I can not find it in datasheet and manual.can you tell me what is the value if the CPU frequency is 100MHz ?
2025-11-05 1:12 AM
For precise time measurement, use timer in capture mode.
The maximum operating frequency may be easily found in the datasheet.
The actual operating frequency is decide on and set by programmer. The maximum is 100 MHz for F411 and 170 MHz for G431.
2025-11-05 1:41 AM
> I need to know the external interrupt response time of GPIO ...
You would need to use an EXTI - capable GPIO (external interrupt) for that. This feature is not implemented for all GPIOs.
> but I can not find it in datasheet and manual.
Look up EXTI interrupt.
The interrupt latency is 12 cycles in almost all cases.
Depending on what you want to achieve, using specific timer features might be a more precise and performant solution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.