2016-12-14 11:28 PM
Hello everyone,
I have the STM32F769I-DISCO board with LCD on it. The CubeMX has options to generate firmware for the following toolchains:
1. EWARM
[requires a paid license]
2. MDK
[works without license but the IDE is lagging on my computer], P.S- I have a gaming machine with beastly performance.
3. Truestudio
[free, the best IDE so far for me. I am able to write code and launch through this IDE]
4. SW4STM32
[This is the worst toolchain. Inspite of being supported by the STM community, it has several bugs. I was unable to compile the firmware generated by cubeMX. It throws lots of errors.]
For some reasons, the printf is not working in Truestudio. That's why I am looking at the most preferred environment for programming this board.
Sorry to say this, but the firmware examples are very bad. Please include examples which will ease our development.
Thanks
Dheeraj
Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-02-05 5:08 PM
Sorry I missed one of your replies. The printf works on Keil with a different board and on a different computer. I was able to use the code posted by Georgeand use the printf through UART. I had some problems with it but I was able to add some print statements and see the output in the COM port.
2017-02-08 3:17 AM
No perfect ID, is a myth.
Those who create such a myth - it is necessary to shoot a little bit.Any selected ID requires knowledge.After receiving the bare metal programming skills - problem disappear selection ID. You will be able to program any ID.// Can directly write in Russian?2017-02-08 4:55 AM
No perfect ID, is a myth.
Those who create such a myth - it is necessary to shoot a little bit.Any selected ID requires knowledge.Quite true.
IDE's are supposed to make things simpler for the 'un-adept'. Actually, they tend to make things much harder once you deviate from the foreseen path ...
// Can directly write in Russian?
Not recommended. Hardly anyone here can read cyrillic letters, let alone decipher words.
I could.
2017-02-08 6:32 AM
Oh yes, I see it.
Re-transfer is difficult to confuse with something else.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.