STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem of porting FreeRTOS to STM32H573I-DK by CubeMX

Hi everyone,I have a STM32H573I-DK and try to port FreeRTOS without TrustZone to this board by CubeMX but suffered from a problem.I installed the X-CUBE-FREERTOS, set TIM17 for HAL Tick and SysTick for FreeRTOS.It will block (or crash?) in vStartFirs...

EyckHuang by Associate II
  • 2896 Views
  • 5 replies
  • 1 kudos

Resolved! STM32G4 Half-Duplex Slave early Complete Callback

Hi, I am using STM32G474RE. I try to read out LTC2440 with the SPI interface. I have configured the LTC2440 as SPI master (In its datasheet the mode of operation is specified as Internal SCK, 2-Wire I/O, Continuous Conversion). The LTC2440 provides a...

IMG_20251202_162259.jpg IMG_20251202_162228.jpg
oeser by Associate II
  • 901 Views
  • 5 replies
  • 2 kudos

Resolved! caches in h7 series

hi, I'm using stm32h745 dual core MCU, in this i want to know about the caches.these I cache and D cache are default enable are it will enable from IOC configuration of M7 core.if not enabled from IOC still these caches will work automatically?due to...

help needed to acquire STM32G474VET6 internal temperature

Hello community,I am new to stm32, and I need to read the temperature from the internal sensor of a stm32g4vet6.I am at the point where I have read many things and have discovered that not all stm32's internal temperature sensors must be used the sam...

phdm by Associate
  • 643 Views
  • 3 replies
  • 0 kudos

Quad SPI Mode 1-1-4 Read Problem

Hi,I'm using OCTOSPI in Mode Quad SPI on a STM32H563ZIT6.  I'm having issues when reading Serial Flash data with a 1-1-4 (6Bh) read, 1-1-4 (32h) write is working fine. Also 1-1-1 read and 1-1-2 read also work fine.  The serial flash is IS25LP032D.  I...

Mike_d by Associate
  • 626 Views
  • 1 replies
  • 0 kudos

STM32H523 QUADSPI W25Q64 External Loader

Hi, I'm trying to do an external loader according ST's MOOC and this forum https://community.st.com/t5/stm32-mcus-products/stm32h5-external-loader/td-p/601134.My code pass on all ST's tests of memory, but when I generate a stldr it does not read on c...

MMira.4 by Associate II
  • 4883 Views
  • 16 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.