STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CommandSet Issue with STM32H7B3 + Parallel NOR Flash

Hi, I have a custom board using STM32H7B3 with the MT28EW128ABA1HJS-0SIT NOR Flash, and I'm getting an error trying to initialize the NOR Flash during HAL_NOR_Init.   /* Get the value of the command set */ ... else // 16 Bit { NO...

wlynn777 by Associate III
  • 2107 Views
  • 2 replies
  • 0 kudos

Resolved! LPTIM current consumption

Hello, For my research work I want to characterize how much current the LPTIM of a STM32U575ZIT6Q consumes when in compare match mode (counting from 0 to 65535 repeatedly).I prorgrammed two very simple codes, one where the counter is not initialized ...

MCU current.jpeg
R.uy by Associate II
  • 1872 Views
  • 1 replies
  • 2 kudos

STM32F407VET6 FSMC to LCD driver

I want to try to interface a 7" 1024X600 display with the STM32F407VET6 chip. I know that the F407 does not have a LTDC so I was wondering if I could use a LCD driver chip that could be wired to the FSMC of the microcontroller. I also plan on using a...

I'm writing the following code: GPIOA-"MODER" 0x400; (set GPIO_MODER_MODE5_0). It's not working! In the debugging window, bit 11 doesn't change and the LD4 LED doesn't switch.

I have Nucleo-G071RB. I want to flash the LED LD4 using CMSIS. Use IAR 8.40I'm writing the following code: GPIOA->MODER |= 0x400; (set GPIO_MODER_MODE5_0). It's not working! In the debugging window, bit 11 doesn't change and the LD4 LED doesn't switc...

VTyut.1 by Associate
  • 4104 Views
  • 3 replies
  • 0 kudos

equation implmentation on STM32F405

I wanted implement  this formula y = a*x^b on the STM32F405 processor. But  can  I do the power multiplication on the STM32F405. Any help on this matter. Thank you

cjaya.2 by Associate II
  • 1465 Views
  • 2 replies
  • 1 kudos

STM32 field firmware upgrade with "CubeProgrammer Light"

Hi everyone,we have taken over the further development and support of a board containing a STM32F407. The board contains a USB port, connected to PA11/PA12, Reset and BOOT0 are connected to push-buttons. So a firmware upgrade by means of the STM32Cub...

Resolved! STM32F070RBT Bootloading via USB

According to AN2606 section 12 we can use USB DFU bootloader as long we have HSE using a 24, 18, 16, 12, 8, 6, 4 MHz crystal. This is missing from section 3.3 of the datasheet. Is there a reason for this?

CWedg.1 by Associate III
  • 1988 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H562 FLASH Prefetch and ICACHE

Hello,I am currently evaluating the STM32H562 device. This devices has an ICACHE (instruction cache) module.Does it make sense to enable both, the ICACHE module and the FLASH prefetch buffer? In the past I already worked with the G0, G4 and F4 series...

Resolved! STM32G473 extended CAN ID never even

I'm attempting to interface an STM32G473 with a VESC motor controller using CAN.I am successfully receiving status frames from the VESC controller, but when I transmit a frame to command it, the ID my scope reads in the frame is not always the same a...

SRP by Associate II
  • 7202 Views
  • 6 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.