2024-01-19 7:19 AM
Hi, I have a custom board using STM32H7B3 with the MT28EW128ABA1HJS-0SIT NOR Flash, and I'm getting an error trying to initialize the NOR Flash during HAL_NOR_Init.
/* Get the value of the command set */
...
else // 16 Bit
{
NOR_WRITE(NOR_ADDR_SHIFT(deviceaddress, uwNORMemoryDataWidth, NOR_CMD_ADDRESS_FIRST_CFI), NOR_CMD_DATA_CFI);
}
hnor->CommandSet = *(__IO uint16_t *) NOR_ADDR_SHIFT(deviceaddress, uwNORMemoryDataWidth, NOR_ADDRESS_COMMAND_SET);
status = HAL_NOR_ReturnToReadMode(hnor);
}
where hnor->CommandSet is read as 0xFFFF, which doesn't match NOR_AMD_FUJITSU_COMMAND_SET or NOR_INTEL_SHARP_EXT_COMMAND_SET so the status becomes HAL_Error and goes to error handler.
Below is the Init & Timing for the NOR Flash:
hnor1.Instance = FMC_NORSRAM_DEVICE;
hnor1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
/* hnor1.Init */
hnor1.Init.NSBank = FMC_NORSRAM_BANK1;
hnor1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
hnor1.Init.MemoryType = FMC_MEMORY_TYPE_NOR;
hnor1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
hnor1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
hnor1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
hnor1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
hnor1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
hnor1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
hnor1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
hnor1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
hnor1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
hnor1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ASYNC;
hnor1.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE;
hnor1.Init.PageSize = FMC_PAGE_SIZE_NONE;
/* Timing */
Timing.AddressSetupTime = 4;
Timing.AddressHoldTime = 20;
Timing.DataSetupTime = 15;
Timing.BusTurnAroundDuration = 15;
Timing.CLKDivision = 16;
Timing.DataLatency = 17;
Timing.AccessMode = FMC_ACCESS_MODE_B;
How can I solve this problem? Any help is appreciated.
2024-01-22 6:50 AM
Hello @wlynn777 and welcome to the Community :),
Could you please check NOR device configuration for MT28EW128ABA1LPC-0SIT NOR Flash, for that I advise you to take a look to stm32h7b3i_eval_nor.c file.
I hope this help you!
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-22 7:37 PM - edited 2024-01-22 7:40 PM
Hi Kaouthar,
Thanks for your reply! I have matched the device configuration & timing with the stm32h7b3i_eval_nor.c NOR driver, but the results are still the same (0xFFFF).
I've also tried to read the manufacturer code & device code of the NOR flash as below:
else
{
*(uint16_t*) 0x60000555 = 0x98;
uint16_t containsQ = *(uint16_t*) 0x60000010 & 0xFF;
uint16_t containsR = *(uint16_t*) 0x60000011 & 0xFF;
uint16_t containsY = *(uint16_t*) 0x60000012 & 0xFF;
/* Get the value of the command set */
NOR_WRITE(NOR_ADDR_SHIFT(deviceaddress, uwNORMemoryDataWidth, NOR_CMD_ADDRESS_FIRST_CFI), NOR_CMD_DATA_CFI);
hnor->CommandSet = *(__IO uint16_t *) NOR_ADDR_SHIFT(deviceaddress, uwNORMemoryDataWidth, NOR_ADDRESS_COMMAND_SET);
status = HAL_NOR_ReturnToReadMode(hnor);
but what should've been QRY (51h, 52h, 59h) is instead (0h, 2400h, 24Ch).
I've also tested the hardware side; address, data, and control pins are fully functional under an oscilloscope.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.