STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747 ADC ENOB Process Variation

Hi,Is there any information available regarding the process variation of the ADC12 ENOB in the STM32H747 operated as a differential ADC? With a custom PCB we are seeing a standard deviation of 2.73 bits, which is quite substantial. On the worst offen...

slc2015 by Associate II
  • 2772 Views
  • 3 replies
  • 0 kudos

STM32U575: Watchdog reset when exit from STOP3 mode.

Hello,in my application, exiting from STOP3 mode is working fine but when the SRAM is over 192K, so getting SRAM2 addresses, exiting from STOP3 mode is forcing watchdog reset (I think when is trying to access a variable placed on SRAM2)  however from...

SMill.8 by Associate II
  • 7255 Views
  • 14 replies
  • 5 kudos

Resolved! STM32F427 Bootloader HSE Signal

Hi, is it necesarry to use a crystal oscilator for DFU USB booltloader for STM32F427zit? Can I use a generator instead of crystal? Marcin

mkuczma by Associate
  • 3207 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H743 Save ADC Output from DMA to RAM to Flash

Hi all, im using Cube IDE STM32H743ZI2 Evaluation boardim curently sampling ADC2 and storing the output at an internal array using DMAthe array size is uint16_t[100,000]my requirements as to store much more data which means i have to use a diffrent m...

shahaf321_0-1707061080066.png
shahaf321 by Associate III
  • 3706 Views
  • 5 replies
  • 3 kudos

Resolved! Revert .ioc file for older CubeIde version

Hello,I recently upgraded to CubeIde 1.6.0 but I am having many new problems when programming STM32h/43: the configurations generation is much slower and it often stops updating all needed files, which forces me to reboot (I could not find a better w...

SSorr.1 by Associate II
  • 5913 Views
  • 4 replies
  • 1 kudos

STM32F439 Ethernet Frame Transmit Jitter

Hello,I have some questions regarding Ethernet frame transmission.1) When is the value of the "ETH_MMCTGFCR" register increased?After calling the "HAL_ETH_TransmitFrame()" function, I noticed that the value of the "ETH_MMCTGFCR" register increased in...

2024-01-31 181125.jpg

STM32 UART stops At High Temperature

Hi,I am Using an stm32f205 on our board. All the Uarts works fine at room temperature. But when the temp increases above 58 degress, messages started get missed in the uarts or sometimes it completely stops sending messages.I am running the board at ...

JThom.15 by Associate III
  • 6172 Views
  • 10 replies
  • 6 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.