2024-02-15 3:53 AM
We want to use the STM32U585QII6Q for a new design, and I want to know what I need to do with the dedicated OPAMP VINM pins on this package. We don't want to use the OPAMPs. Do I leave these dedicated pins floating or should I connect them to GND?
I checked the 'STM32 microcontroller GPIO hardware settings and low-power consumption' application note, but it doesn't state anything about dedicated OPAMP input pins.
2024-02-15 12:48 PM
GND should work fine. The op-amp common-mode range is 0 to VddA, so the input multiplexer should be able to cope with anything in that range.
Personally I would put a series resistor on my pcb on the path to Vss if this is a prototype. Although you might not have thought that you need an op-amp, you might later decide it is handy for some as-yet-unknown reason.
2024-02-15 1:22 PM
I think keep OPAMP_EN disabled and keep all unused GPIO in analog mode is the way to go.OPAMPOPAMP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.