STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RXNEIE needed for dma request?

Hello, i am trying to interface TI's ADS8910 (18bit SAR ADC) to an STM32F730 via normal SPI, since i am unsure whether QSPI will work.I want to achieve the full 18 bit @1MSa, which is possible when working with 54MHz (/2 APB2 prescaler on the F730 wh...

Resolved! STM32F303 USB

Hello,I'm working on a cutom made board controlled by an STM32F303ZET, I figured out that I forgot to pull up D+ for USB communication, even doing it externally keep showing me this error. I tried to pull up the D+ using 3.3V directly and also by pul...

EL_HACHIMI_0-1708698094232.png

STM32H755 Reset Reason

Hello,I am using an STM32H755 dual core chip and occasionally, our reset reason (RCC_RSR) is decoding to have only theD1RSTF bit and D2RSTF bit set.  Per the documentation, it does not seem this is an expected combination alone...Per table 56 in sect...

scuba by Associate II
  • 1563 Views
  • 1 replies
  • 0 kudos

equivalent application note

HI, Is there an equivalent application note or similar information about sleep modes for the F0 series?https://www.st.com/resource/en/application_note/an4365-using-stm32f4-mcu-power-modes-with-best-dynamic-efficiency-stmicroelectronics.pdfCheers, Cla...

Resolved! Stm32 azure rtos

Hi, I am new to stm32 microcontroller. I am finding difficulty to render my html page using azure rtos. As I have seen the example of stm32f429zi nx_Webserver. First of all  I could not find html files in the example folder.However with other GitHub ...

STM32H5 I3C Target don't send ACK when receive header

My I3C target don't send ACK after controller send an arbitration header ,and it will generate a DOVER flag and ERRF flag. ex.Send HAL_I3C_Ctrl_IsDeviceI3C_Ready before controller transmit data.Send HAL_I3C_DIRECTION_READ and so on

Sunwaz by Associate III
  • 2423 Views
  • 4 replies
  • 0 kudos

3-wire SPI Configuration

Hello,Currently i'm working on STM30F030 controller.I want to connect TFT display with this controller, display has three pin for SPI (SDA,SCL & CS) and used only for write operation.so how to configure controller for 3-wire SPIIf i have to connect...

SPraj.15 by Associate II
  • 2199 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.