STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to check the authenticity of STM32 chips?

Hi everyone, I'm deep into developing a project that is not only a passion but also a venture I'm financially invested in. I recently ordered a small batch of 50 PCBAs equipped with STM32L476RET6 microcontrollers from a well-known Chinese manufacture...

STM32L476RET6.JPG
AChap.1 by Associate III
  • 5795 Views
  • 6 replies
  • 5 kudos

stm32wb55 ADC read error

Hi all,I am using an stm32wb55 neucleo board for a wearable based project. I am using ADC1-IN1 to read the adc raw value from MCU pin PC0 of wb55 board.  A voltage divider circuit was connected to scale down the BAT voltage from (4.2-3.7) to (1.8-1.5...

Resolved! Error in STM32G4 reference manual RM0440, revision 7 (February 2022), section 44.3.3 Message RAM of FDCAN peripheral

Figure 669. Message RAM configuration clearly shows that the message RAM is 0x350 bytes long which corresponds to 212 32-bit words. But later the following example is used to show, how the message RAM of FDCAN2 follows message RAM for FDCAN1:As an ex...

VMich.1 by Associate II
  • 2312 Views
  • 2 replies
  • 0 kudos

Resolved! Error in Reference Manual - RM0440 Rev 4 - Page 358, section 9.3.13, "Using the HSE or LSE oscillator pins as GPIOs"

The word "OSC_IN" is missing from the following sentence:"When the oscillator is configured in a user external clock mode, only the pin is reserved for clock input and the OSC_OUT or OSC32_OUT pin can still be used as normal GPIO."Should say: "...onl...

Resolved! Error in Reference Manual!! RM0440 Rev 4 page 1341

Table 285, register map for general timers, TIMx_SMCR, contains two errors:This shows SMSPE in bit 25, I believe it is actually in bit 24.Also it shows SMSPS in bit 26, I think it is actually in bit 25.Please let me know if I'm mistaken. Thank youRM0...

Resolved! LwIP webpage not updating

Hello, I am using LwIP alongside a STM32F7. I am very new to network programming and I was wonder why the webpage is not updating when I modify the html code. If I visit the page via the IDE, the changes are there but on a live version of the site, n...

Carrcl by Associate II
  • 3483 Views
  • 7 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.