STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC data is only being read alternately (TIM1 + DMA)

"Hi,I am trying to read an ADC value from the feedback of a PWM signal generated via TIM3 PWM.TIM1 generates a PWM signal with 4 channels, including complementary channels. The CCR value updates from the Sine table using DMA.The ADC is being read whe...

kk.jpg

stm32h7 receive audio over udp

hi, that's the first time a i wrote to this comunity because i'm stuck with this *** problem since one week right now, i made a custom board with stm32h750vbt6 , 4 stereo audio dac and 2 4ch audio adc, eth phy , clock gen ic and etc.. now my idea was...

eman8388 by Associate
  • 1030 Views
  • 0 replies
  • 0 kudos

Possible to read program stored in STM32F103C8T6 ?

Hello everyone,I bought a tool that uses a STM32F103C8T6 with a program on it to transmit some CAN data. I would like to read the program that is currently on the tool and edit it.Is it feasible ? Or is the memory protected ?Thanks in advance for you...

Math86 by Associate II
  • 13034 Views
  • 21 replies
  • 0 kudos

Stack in SRAM2 on STM32F413VGT6

Hi guys,I need your collective intelligence, because I am a bit lost on the information given by the ST datasheets and reference manuals.Backstory: on a few of our prototypes we started to see random failing behavior and investigated quite a bit. The...

Following AN4666 (reception) for STM32G474

Hi all,I am currently working on a project where an 8 bit bus of 32 MHz is sent to a STM32G474, which has to be saved for 8kB at a time followed by that data being sent over SPI. I have got the SPI part working fine, my question is mainly regarding A...

Connect battery to BL475E-IOT01A Discovery Kit

Hello, I want to supply my St Iot discovery kit board with a battery supply, I have changed the header pin to 5V_VBAT. As i am connecting my battery to the Vin and gnd pins the red LED keeps blinking and LD5 is off.  Kindly give some suggestions how ...

Arhum_29 by Associate II
  • 1322 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.