STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f103 samples per second adc

Hello, I'm using a stm32F103 to read 10 channel from the ADC in continuos mode. The ADC clock is 12Mhz and the sampling time is 28.5 cycles for all channels. the convertion time for one channel is ((28.5+12.5)/12Mhz) = 3.41 us. Since i'm using adc in...

fdin by Associate II
  • 3445 Views
  • 5 replies
  • 0 kudos

Resolved! Difference between nominal and data bit time FDCAN parameters

Hello,I am developing a CAN bus application.I am new to the FDCAN peripheral and I haven't understood the difference between nominal bit time parameters and data bit time parameters.Which of these two groups of parameters should I configure to obtain...

CTabo.1 by Senior
  • 4653 Views
  • 4 replies
  • 1 kudos

Resolved! How to configure external memory in NUCLEO-H745ZI

Hello Team,I want to add external memory to NUCLEO-H745ZI board. In that board i have configured 2SPI, Ethernet (without RTIOS) and Timmer for that I need huge memory. This there any configuration or steps to add external memory to board. Best Regard...

ggowd.1 by Associate III
  • 13229 Views
  • 25 replies
  • 4 kudos

Resolved! CANFD configuration with CAN 2.0 devices

I am using CANFD with an STM32H7 and a transceiver that is compatible with CANFD and CAN 2.0 (ISO1044BDR).I can see that in the configuration the CANFD can be used as a CAN 2.0. What I want to know is what is the easiest way to integrate the flexibil...

__silardg by Associate III
  • 7760 Views
  • 7 replies
  • 3 kudos

ST Bootloader behavior when flash is not programmed

Hi everyone!I found the following diagramm in AN2606 and my understanding was, that the bootloader will be executed when there is no valid content in flash memory.I know that boot pins or a jump from user code can be used to enter the ST bootloader, ...

kf_SEA_0-1711459809997.png
kf_SEA by Associate II
  • 1199 Views
  • 1 replies
  • 0 kudos

How to Include HAL Libraries into Already Existing Project

Hello,I am using an STM32F407G-DISC1 to run an open source program called Picovoice. More specifically their project at the following link (https://github.com/Picovoice/picovoice/tree/master/demo/mcu/stm32f407/stm32f407g-disc1). Unfortunately they do...

GSkoumal by Associate II
  • 8334 Views
  • 8 replies
  • 1 kudos

[Resolved] USART Tx pin sinks rx pin. HAL UART bug?

Edit: I found the problem, and it is of course my own fault. Careful reading of the transceiver chip datasheet reveals that the Rx pin follows the Tx pin by design on some models, including mine. Leaving this post up for posterity. I'm having an issu...

AntonL by Associate
  • 1433 Views
  • 0 replies
  • 0 kudos

Clarify stack management on STM32H7 / cortex M7

Hello,I'm a bit confused about stack management on Cortex M7.In my SW I only use the MSP.I understood that the MSP can only be modified with a MSR instruction. However the SP can be modified with a "simple" LDR instruction.Does that mean that when I ...

Gpeti by Senior II
  • 1475 Views
  • 1 replies
  • 0 kudos

Resolved! AN6091 ('L0->'U0 migration) comments

This is not a discussion on the 'U0 as such (that'd need some time to sink in); just comment on the 'L0->'U0 migration document, AN6091. It's a very detailed and extensive document, and following items are just relatively insignificant minor issues/t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.