STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No target found after first flash

I have a board using STM32F103CBT6 chip.  After flashing the board once (through CubeIDE v1.14.0 with ST-Link v2) I cannot flash it again and keep getting the message "No target found".  Here's a snapshot of the chip circuit:  When I power up the boa...

skip_shane_0-1711656751619.png

Resolved! RTC Alarm under VBAT Conditions

From what I understand, a STM32L433RCT3 MCU powered by VBAT pin will shutdown except for RTC and backup registers.1. I'm wondering if the RTC Alarms can trigger during the VBAT period?2. Will any code execute from the RTC Alarm interrupt during VBAT?...

MVeen.1 by Associate II
  • 1397 Views
  • 1 replies
  • 0 kudos

Resolved! Flash memory programming

Hello everyone, iam using nucleo-U575ZI-Q board and trying to do Flash programming. I want to write the data in to the flash and read the data from the flash. I've written the code but something is going wrong with it. Could someone please help me in...

_JITH_ by Associate
  • 5133 Views
  • 4 replies
  • 0 kudos

STM32U5 QFN Availability

Is there anywhere tog go to find out when parts that are not currently in stock will be?Some parts even though they are a new product line seem to have NEVER had any stock, and I though the covid supply issues were now sorted.Specifically at the mome...

Resolved! How to design an USB OTG interface

Hello everyone,After several hours of searching, I haven't found a working example of an electronic schematic for interfacing a USB OTG port with an STM32 F7.Furthermore, the documentation provided "AN4869 Rev6" by ST is not clear enough to produce a...

Boris19_1-1711035327036.png Boris19_0-1711035303947.png Boris19_2-1711036218467.png
Boris19 by Associate III
  • 19604 Views
  • 8 replies
  • 0 kudos

Resolved! MTBF or FIT for component STM32F446RET6

Dear all, I need to know : 1.MTBF(Mean time between failure)2.Longevity.3.Shelf life or storage life.For component: STM32F446RET6I already try a online support, but the site show me “we can’t save this record ”.Can anybody help me? 

SAI - how to synchronize the data transmit between 2 blocks

Hi!I am still playing with the SAI of my STM32F446RE. It has one SAI (SAI1) which has two blocks, A and B.The idea is to use the two blocks synchronously in TDM mode to transmit in total 8 slots, 4 slots for each block.I can get it to work fine, thou...

SLasn.1 by Senior
  • 6853 Views
  • 10 replies
  • 0 kudos

STM32 U5 ADC (multi channel) + timer + DMA

I am working on development project using NUCLEO-U575ZI-Q.The application is to scan multiple analog signals (4) signals using ADC1 (14 bit). The ADC triggered periodically using Timer 1. The results to be transferred to memory using DMA. Any sample ...

Tvoge.1 by Associate II
  • 6464 Views
  • 5 replies
  • 0 kudos

Resolved! CAN Communication issue with STM32F4

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file can.c * @brief This file provides code for the configuration * of the CAN instances. *********************...

JDOG_0-1710445814919.png JDOG_1-1710446081374.png
JDOG by Associate III
  • 12497 Views
  • 19 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.