STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F746 QSPI XIP with TouchGFX and FreeRTOS

Hello All, I am very beginner in embedded technology. I would like to learn and implement XIP.Currently I am working on a project which uses STM32F746 discovery board and uses TouchGFX and FreeRTOS. It uses qspi in memory mapped mode to store the fon...

pitbull by Associate III
  • 3351 Views
  • 4 replies
  • 1 kudos

STPM33 spi read issue

I am using STM32 H563 Nucleo board to read the configurational register (address = 0x24) of STPM33 evaluation board using SPI protocol but while debugging the code i am getting random values on each transmission. Firstly i am transmitting an bytes {0...

Dev_Oza_0-1712052899008.png Dev_Oza_1-1712052912298.png Dev_Oza_2-1712052924621.png Dev_Oza_3-1712052938852.png
Dev_Oza by Associate
  • 1468 Views
  • 0 replies
  • 0 kudos

Sometimes HAL_SPI_TxRxCpltCallback() is not getting called.

We are using STM32G4 Series microcontroller for SPI comm. as slave with microprocessor.For SPI TX operations sometimes we are seeing that callback function HAL_SPI_TxRxCpltCallback() is not getting called even though we are seeing that data is transm...

_legacyfs_online_stmicro_images_0693W00000bkHdKQAU.png
PDhar.1 by Associate II
  • 6094 Views
  • 7 replies
  • 0 kudos

Resolved! STM32U5xx: SPDIF out - how to configure?

I am struggling since days to get "my audio" out via SPDIF (electrical).What I see on scope (there is a voltage divider and cap for DC-free on PC12, Vpp is 0.6V, approx. 75 Ohm impedance):It makes sense - but my SPDIF receiver (a STM32F769I-DISCO boa...

MCU_SPDIF.png
tjaekel by Lead
  • 4573 Views
  • 5 replies
  • 0 kudos

Resolved! ADC Calibration doesn't complete on STM32G0C1RE.

Using HAL_ADCEx_Calibration_Start() to calibrate the ADC. This function always returns HAL_ERROR.Debugging shows its failing after it collects the 8 samples and attempting to disable the ADC is timing out.  (ie.  if ((HAL_GetTick() - tickstart) > ADC...

BrianB by Associate II
  • 9703 Views
  • 11 replies
  • 4 kudos

How to flush cache in CubeF7 Flash EraseProgram example?

In the CubeF4 Flash EraseProgram example (STM32F4-Discovery/Examples/FLASH) there is this section after the erase:/* Note: If an erase operation in Flash memory also concerns data in the data or instruction cache, you have to make sure that thes...

osiris81 by Associate
  • 3528 Views
  • 4 replies
  • 0 kudos

stm32l431rct6

I am following the tutorial from https://www.youtube.com/watch?v=I9KDN1o6924&t=384s the tutorial(32F746GDISCOVERY) User manual has showed MicroSDcard_detect is pin PC13.I can not find my pin name of stm32l431rct6 Datasheet for MicroSDcard_detect pin....

Jacob3104_0-1711997870568.png
Jacob3104 by Associate II
  • 1300 Views
  • 1 replies
  • 0 kudos

Storing data in the option byte of STM32 memory.

Hi,1.Can I use option bytes to store the data(eg: Serial number, values storage etc).is It possible if so please share the available resource link/ example for reference. I am using STM32G491RE MCU.I want to write some data in to option byte memory a...

Resolved! STM32L431CCY not reliably booting

I made a little proof-of-concept board for the L431, as I wanted to see what it would take to do a BGA design. I've been able to program is using the STM32CubeIDE, but the board won't boot reliably.STM32CubeIDE v1.13.1Jlink Plus Compact0.1uF Bypass c...

sethkaz by Associate III
  • 1709 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.