STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Isolation between digital 3.3V and Analog 3.3V supply

Hi @Peter BENSCH  Greetings again. I am using STM32H5 and STM32G4 series MCU in my project. As per the datasheets and application notes, it is recommended to isolate analog and digital supply voltages with a proper ferrite bead or a zero ohm resistor...

Wrong timer section identifier in manual (G431RBT6)

I think there are some wron identifiers?After reading the manual and seeing the tables i think it must be "tim_ti2_in0", "tim_ti3_in0" and "tim_ti4_in0" on page 1223? Also in the table on page 1081, there is a "tim_ti2_in[15:1]" that should be "tim_t...

Tobe by Senior III
  • 1179 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G431 tim_ker_ck, tim_pclk source

I'm looking into calculating the timings for the brk filters for the TIM1 periphery. Mentioned there is the "tim_ker_ck" and the "tim_pclk" respectively.I cannot seem to find any information on where these come from.The clock tree in the RM says that...

DMeie.2 by Senior II
  • 4970 Views
  • 10 replies
  • 7 kudos

Resolved! NUCLO-H755ZI-Q Unable to debug CM4

Hi community,I build and program both CM without error and debugger configuration as in the AN5361 .The Nucleo- runs with maximum frequency  480 MHz, and Power supply:  HAL_PWREx_ConfigSupply(PWR_SMPS_2V5_SUPPLIES_LDO);  __HAL_PWR_VOLTAGESCALING_CONF...

Vero by Associate III
  • 3280 Views
  • 4 replies
  • 0 kudos

Resolved! Drop voltage SCL I2C

Hello,I have a very strange behaviour with the I2C bus of a STM32G431.I try to communicate with a MLX90393 of Melexis. I had some problems to get the measurements, after a Start measurement. The MLX90393 returned an error code. So I checked the signa...

0693W000007ZmIBQA0.png 0693W000007ZmIVQA0.png
alxrey by Associate II
  • 4794 Views
  • 6 replies
  • 0 kudos

Resolved! Register programming GPIOA->(AF07<<4) and (AF07<<8)

hi come across these code using register programing, STM32F411 Nucleo bd, anyone can advise how does the (AF07<<4) and (AF07<<8) relate to UART2 PA2 & PA3? please advise..  #define AF07 0x07 GPIOA->AFR[1]|=(AF07<<4)|(AF07<<8); //ALT7 for UART2...

Resolved! STM32G070 DMA memory to memory software trigger

Hi,I have read thoroughly RM0454, STM32G070CB datasheet and AN4187 in order to understand how to configure the DMA and DMAMUX in order to feed the CRC peripheral with FLASH data using the DMA (with CPU it is working but way slower than expected).I do...

Kraal by Lead
  • 7487 Views
  • 8 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.