STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! usb otg voltage level shifter

hi ,i gone through usb pcb guidelines and other forum discussion but i couldn't catch my doubt .1). Incase of Using USB Virtual Com Port D+ (PA12) & D - (PA11) pin can be directly connect with Computer USB port  without level shifter ??? During the  ...

MMARI1_0-1713601726547.png MMARI1_1-1713602790786.png MMARI1_2-1713603479534.png
MMARI.1 by Senior II
  • 2220 Views
  • 2 replies
  • 0 kudos

Resolved! CRC32 MPEG2 configuration for ST32C0x1 CRC driver

HiI'm trying to understand how to configure the hal/peripheral to evaluate the CRC32 MPEG2 over a block of datas.I'm comparing the result with this site where as input I've used the vector 0x01, 0x01. Expected result is 0xD66FB816https://crccalc.com/...

STDoom by Associate II
  • 2592 Views
  • 2 replies
  • 3 kudos

Resolved! STM32H7 : Using the DMA to transfer burst of Can-Bus data

Looking at the FDCAN peripheral application note (AN5348), I don't see any mention of using the DMA. I'm interested in transmitting 30 8-byte messages every second via Classic-Can 2.0.   Since the peripheral's FIFO isn't that deep, I was thinking of ...

bnguy.1 by Associate III
  • 2182 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F405 Can not connect to target

Hello All, I Hope you are well.I am facing a problem that I spent A LOT of time on. I designed a custom board featuring the STM32F405RGT6 but i cannot connect to it at all.. I will attach the schematic and the board's pictures below. (The schematic i...

photo_5839067125233336211_w.jpg photo_5839067125233336220_y.jpg
Mhushki by Associate III
  • 17072 Views
  • 27 replies
  • 2 kudos

STM32F4 Using FileX : Can It Be Used Independently?

Hello, community! I'm a new here .I am developing STM32F4 using STM32CubeIDE(1.14.1), and I want to use the FileX without ThreadX.  However, it seems that this is not possible in CubeMX. The FileX for the F4 series requires ThreadX, and if ignored, t...

屏幕截图 2024-04-20 205243.png 屏幕截图 2024-04-20 205551.png
cashews by Associate
  • 1565 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.