STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 cryptographic firmware library for STM32U5

Hey,in the past we used a STM32F4 and in the new Gen I will use the a STM32U5 and there is my questen about the cryptographic firmware in the past we could use the libSTM32CryptographicV3.0.0_CM4_GCC.a but now is there also a Lib for the stm32u5? 

Resolved! Timer's Combined Channels - Encoder Mode

Hello, I'm using the nucleo-h743zi2 board.When obtaining the value of TIM2->CNT (or TIM5->CNT) through the combined channels of TIM2 or TIM5 on this board, without any special settings, I can perceive the encoder rotating in reverse as a negative val...

HMsDobby2 by Associate III
  • 2349 Views
  • 1 replies
  • 1 kudos

STM32F407 Measuring tie between 2 impulses

Hey. I am working on a task which requires to measure time between 2 different impulses with high precision. We have custom board that generates output pulse based on the capacitor and resistor values. The Input is LOW to HIGH impulse (Green color on...

LPetr1_0-1714725999122.png LPetr1_2-1714723304279.png LPetr1_1-1714723277892.png LPetr1_3-1714723402569.png
LPetr.1 by Senior II
  • 6756 Views
  • 9 replies
  • 1 kudos

Resolved! Get STM32H735G-DK out of deadlock!

I can not connect my STM32H735G board via ST-Link anymore. "no stm32 target found". I tried "connect under reset" (ST Link Utility and ST programmer) as well as connecting boot0 to VDD. Any idea how to erase the flash and start over? Cheers Stefan

ADC same values in Vref and CH0 (STM32F103C8T6) (CubeIDE)

Hello everyone! I can't figure out what my mistake is, from the next code, I have the same values for CH0 and VREF (I read others' replies but they don't work for me).What I'm doing wrong?//------------------------------------------------------------...

andresfir by Associate II
  • 2318 Views
  • 4 replies
  • 0 kudos

SDIO and SD fat access example?

Posted on February 09, 2012 at 01:06Hi Chaps,Going slowly mad trying to get Chan Fat working with the sdio libs on a stm32f4.I'm using the most recent (1.0.0) library for the F4, and the low level access demo within that library builds and (at least...

natblist by Associate
  • 31846 Views
  • 84 replies
  • 0 kudos

STM32U5 Bluetooth and Camera

Hey all,Would I be able to use a Bluetooth module to view video stream from camera module in order for user to view camera feed while setting camera up in the field? I only need to see video stream when setting camera up, after that the camera will t...

Fail to adress memory

Hello, I'm attempting to establish communication between an STM32L552CET6 microcontroller and an external flash memory. When I manually initiate communication, the component responds to the microcontroller, indicating no hardware issues. However, whe...

flash memory issue.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.