STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H503 ADC1 DS14053 Rev 4 vs. RM0492 Rev 3

There seems to be a documentation error between DS14053 Rev 4 and RM0492 Rev 3.  In the data sheet, section 3.17, table 3, "ADC Features" we see a different set of features compared to the reference manual, section 19.3, table 107.  The data sheet cl...

STM32H743VGT6 how to use slave I2C+DMA

STM32H743VGT6 how to use slave I2C+DMACurrently, this usage is fine. However, when using the DMA function, it will trigger an ER interrupt.HAL_I2C_Slave_Seq_Receive_DMA, How to use it? Are there any examples?// 从机地址匹配回调函数 void HAL_I2C_AddrCallback(I2...

AngusHZ by Associate II
  • 221 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F4: OSC_OUT as GPIO when HSE in Bypass mode

ST moderator: post split from this thread. Hello mƎALLEm, Thank you for your confirmation on this issue. I would like to provide some additional information. I have also encountered the same problem on the STM32F405RGT6. In STM32CubeMX, when I config...

Analog Signal Validation

Hi, we have purchased stm32h750vbt6 microcontroller for analog signal validation with 10k potentiometers to integrate with game controller joystick especially joy.cpl using windows 10 OS.   We have dealt with DMA Circular mode configuration pointing ...

Resolved! stm32h7 with integrated usb hs phy

is there a way to search for which stm32h7 mcus have integrated HS usb phy?the mcu finder product selector doesn't have such filter, is there an app note, a product brief or anything like that?How is one supposed to find such a controller? (besides m...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.